How long a user pattern can we make on the N4901/2/6B?
The N4901/2/6B can store user patterns with a maximum length of 32 Mb.
Pattern resolution values define all possible user pattern lengths below 32 Mb. For example, standard patterns can only be increased from 256 kb to 512 kb in multiples of 8 bits. This is also referred to as granularity. The following table lists all pattern resolution values.
Pattern length (standard) | Pattern length (alternate) | Resolution |
---|---|---|
<= 32 kb | 1 bit | |
2 bit | ||
> 128 kb | > 64 kb | 4 bit |
> 256 kb | > 128 kb | 8 bit |
> 512 kb | > 256 kb | 16 bit |
> 1 Mb | > 512 kb | 32 bit |
> 2 Mb | > 1 Mb | 64 bit |
> 4 Mb | > 2 Mb | 128 bit |
> 8 Mb | > 4 Mb | 256 bit |
> 16 Mb | > 8 Mb | 512 bit |