Understanding the ParBERT Generator/Analyzer Modules
One of the most frequently asked questions is "How do the data modules work?" It actually isn´t worded that way. Instead it might be "Why can´t I set the frequency to 2.5 Gbps when the segment resolution is 2?" or "Why do the windows turn red when I lower the clock frequency to 300 Mbps?" or "Why won´t the ParBERT sync?" Ultimately, it boils down to a need to understand the structure and functionality of the memory, sequencer and multiplexer found in the generator/analyzer module, as well as the methods of synchronization used. To learn more about this see the Related Links.