Does Keysight Intuilink VNA operate with the 8753D Network Analyzer?
Keysight IntuiLink VNA operates properly with 8753D VNAs equipped with firmware revision 06.14 or revision 07.14 only.
To check the 8753D firmware proceed as follows:
Depress the front panel SYSTEM hard key (HK), followed by the SERVICE MENU soft key (SK), and finally the FIRMWARE REVISION (SK). The analyzer front panel display will indicate "HP8753D.xx.xx", where xx.xx is the 8753D firmware revision.
Please note that a limitation of using IntuiLink for VNA version 1.3 with 8753D 6.14 is that the feature for saving an instrument state with a calibration or restoring the same to the 8753D does not work correctly. This issue with IntuiLink will not be resolved, as 8753D is an obsolete instrument. Please consider using IntuiLink for VNA with 8753E/ES/ET or 872xES/ET instead, as this issue does not occur when the software is used with 8753E or 8720E series - models that are still supported by Keysight.
Keep in mind that when using the IntuiLink for VNA toolbar with 8753D (running 6.14 firmware or later), you can still do perform tasks such as screen capture and measurement data transfer into Microsoft® Excel or Word.
Microsoft is a U.S. registered trademark of Microsoft Corporation.