How do I use the Service Request method (SRQ) to determine if the X-Series, ESA and PSA Signal Analyzers measurement is complete or has an error me...
Disclaimer:
You have a royalty-free right to use, modify, reproduce and distribute the Sample Application Files (and/or any modified version) in any way you find useful, provided that you agree that Keysight Technologies has no warranty, obligations or liability for any Sample Application Files.
Description:
The example program, SRQ.C, is writtten for the X-Series, PSA, and ESA SIgnal Analyzers. The program demonstrates how to:
- Set the service request mask to assert SRQ when a measurement is uncalibrated or an error message has occured.
- Initiate a sweep and wait for the SRQ interupt
- Poll all instruments and report the nature of the interrupt on the spectrum analyzer
Instrument Requirements:
X-Series, ESA, or PSA Analyzer
Languages Supported:
ANSI C or Visual C++
Additional Requirements:
None
Revision Date:
January 2004
Download Instructions:
Download the file below: Service Request Method (SRQ)
Procedure:
Compile the program using Visual C++ 5.0 or 6.0 or other ANSI C compiler. Set the GPIB address of the instrument to address 18. Connect the GPIB cable and execute program.
Learn more about Keysight ESA Spectrum Analyzer