For my ESA/PSA/EMC Series Spectrum Analyzer or E4406A VSA Series Analyzer how do I serial poll to determine when an auto-alignment is complete usin...
Disclaimer:
You have a royalty-free right to use, modify, reproduce and distribute the Sample Application Files (and/or any modified version) in any way you find useful, provided that you agree that Keysight Technologies has no warranty, obligations or liability for any Sample Application Files.
Description:
The example program SerAlign.c, is writtten for the PSA and ESA and EMC Series Spectrum Analyzers and the E4406A VSA Series Analyzer. The program demonstrates how to perform an alignment and use serial polling to determine when the alignment is finished. This allows the user to perform an alignment and not tie up the GPIB bus while waiting for the alignment to complete.
Instrument Requirements:
ESA or PSA Series Spectrum Analyzer or E4406A VSA Series Analyzer
Languages Supported:
ANSI C or Visual C++
Additional Requirements:
None
Revision Date:
October 2001
Download Instructions:
Save the text from PSA/ESA/E4406A Serial Poll Alignment Routine for C Programming file to disk and view using a text editor.
Procedure:
Compile the program using Visual C++ 5.0 or 6.0 or other ANSI C compiler. Set the GPIB address of the instrument to address 18. Connect the GPIB cable and execute program. The C program will start the alignment routine on the instrument and poll it every second to determine if the alignment routine is complete.