Keysight Technologies Collaborates with Bluetest on NarrowBand-Internet of Things Over-the-Air Test Solution

  
  

Provides powerful, cost-effective test solution for evaluation of internet of things device performance

Highlights:

  • Uses Keysight's UXM wireless test set, which supports the very latest narrowband-internet of things (NB-IoT) specification, as well as enhanced machine-type communication (eMTC) Cat-M1
  • Implemented in Bluetest Reverberation Test Systems, which are ideally suited for testing of IoT device performance since there are no traditional test zone limitations

SANTA ROSA, Calif., Sept. 26, 2017

Keysight Technologies, Inc. (NYSE: KEYS) today announced the collaboration with Bluetest on the successful creation of a narrowband - internet of things (NB-IoT)) over-the-air (OTA) solution for use in Bluetest Reverberation Test Systems (bluetest.se/products/chambers). The solution, used by one of Japan's top operator customers, demonstrates the market leading position of both companies in NB-IoT test.

"We are excited to announce this collaboration with Bluetest," said Kailash Narayanan, vice president and general manager of Keysight's Wireless Devices and Operators Segment. "The work reinforces our leadership position for Cellular IoT (CIoT) device workflow testing, from the early stages of R&D and conformance, into antennae OTA solutions."

"We're very satisfied with the close cooperation from Keysight that enabled us to meet the market demands on early creation and support for testing of NB-IoT devices," said Klas Arvidsson, product manager for Bluetest's OTA solutions. "This delivered a powerful test solution for evaluation of IoT device performance, such as transmitted output power and receiver sensitivity, which is important when striving for good connectivity, particularly in challenging link budget conditions."

NB-IoT technology uses existing cellular network infrastructure to deliver excellent coverage and reliable connectivity. This approach is becoming adopted by major worldwide operators. The OTA test is critical for operators to qualify the interoperability and compliance of their NB-IoT devices. This is particularly important when a third-party enclosure is used with the device since the antenna coverage effects could be limited.

Bluetest Reverberation Test Systems are especially well suited for testing of IoT devices with their capability of measuring larger test objects since there is no traditional test zone limitation in the chamber.

Recent enhancements to the UXM wireless test set support the very latest NB-IoT specification, which supports RF measurement, power consumption and end-to-end data test—making it an ideal choice for a wide range of wireless user equipment—from IoT devices to smartphones.

Additional Information

More information about Keysight's UXM wireless test set is available at www.keysight.com/find/UXM. High-resolution images are available at www.keysight.com/find/UXM_images. Videos demonstrating the UXM's versatile capabilities are available on YouTube. Contact Keysight at www.keysight.com/find/contactus for E7515A UXM pricing and delivery information.

About Keysight in Wireless

From WLAN to LTE-Advanced to the new 5G technologies, Keysight is focused on tackling the toughest design and test problems in the industry with the broadest range of solutions. With the most advanced electronic measurement solutions consisting of powerful software tied to both benchtop and modular hardware, engineers are able to get greater insight into design and test from simulation to R&D, from validation to manufacturing, from conformance to deployment. With experienced engineers in significant roles in cellular and WLAN standards groups and hundreds of application engineers all over the world, Keysight expertise is there to solve customer problems. Additional information is available at www.keysight.com/find/UXM and www.keysight.com/find/cellular.


About Keysight Technologies

Keysight Technologies is a leading technology company that helps its engineering, enterprise and service provider customers optimize networks and bring electronic products to market faster and at a lower cost. Keysight's solutions go where the electronic signal goes, from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $2.9B in fiscal year 2016. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.

About Bluetest

Bluetest is the pioneer and market leader in reverberation chamber technology for over-the-air (OTA) testing of wireless devices and small antennas. Bluetest's innovative RTS products have been adopted by the largest mobile phone manufacturers, network operators, antenna manufacturers and other providers of wireless solutions. For more information, visit www.bluetest.se.

# # #

Contact:

Geri Lynne LaCombe, Americas
+1 303 662 4748
geri_lacombe@keysight.com

Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com

Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com