CX3300 Device Current Waveform Analyzer
Quick Operation Guide
File
How to save the data
How to load the data
What types of data formats are supported on the CX3300 ?
Setup
How to change the horizontal scale and position
How to change the sampling rate
How to change the memory depth
How to change the 14-bit or 16-bit resolution
How to change the vertical scale and position
How to change the current range
How to set the bandwidth limit
How to minimize the offset current
How to perform a Skew adjustment
What determines the effective bandwidth of the instrument ?
How to zoom in on the waveform
How to use the waveform memory
How to overlay multiple acquisitions
Trigger
How to set the trigger
Measure
How to apply a Measurement Function
How to apply the A-B marker
How to add an Annotation
Analyze
How to perform the FFT ( Fast Fourier Transform )
How to view the integral value of a specified area
How to apply the Power and Current Profiler
How to apply the post-filter
Utilities
How to perform User calibration
How to check the firmware revisions
How to simulate the 50 MHz or 100 MHz bandwidth option on the mainframe with the 200 MHz option
Where to find the Online help