=============================================== README.TXT EasyEXPERT for B1500 Update =============================================== This document contains the following: * Software Requirements * Update Instructions Software Requirements ===================== In order to update the EasyEXPERT Rev. A.05.04 or prior revisions to Rev. A.05.50 or later revisions, the following software are required. - Microsoft Windows Installer 3.1 - Microsoft .NET Framework 3.5 Service Pack 1 NOTE: If your computer does not install all required software, install them in the above sequence. If your computer does not install a software, install it and the following software. For example, if your computer does not install Microsoft Windows Installer 3.1, install it, and Microsoft .NET Framework 3.5 Service Pack 1 in this sequence. The required software are stored in the EasyEXPERT Updater Prerequisites folder in this Package. Update Instructions =================== To update the EasyEXPERT for B1500, follow the procedure below. 1. If the downloaded file is saved to a PC, copy it to B150xA by using a media such as CD-R/DVD-R/USB memory. 2. On B150xA, if you see [Start EasyEXPERT] button on the screen, close the window by clicking "x" button on the window title bar. 3. Expand the contents of the downloaded file into a working folder as follows. a) Go to the folder where the downloaded file is saved and open the folder. b) Place the pointer on the downloaded file and click the mouse right bitton and select "Extract All...". NOTE: If any unzip tool is installed, the above may not work. In this case, follow the instruction of the tool. Below is an example for the tool "winzip". - Firstly double-click the donloaded file, then click "unzip" in the menu bar. Then specify the folder and click "unzip". 4. Double click the index.html file in the expanded folder. 5. Click "Update EasyEXPERT" icon and follow the instructions of the setup wizard. 6. Wait for installation to complete, and restart the B150xA. Microsoft and Windows are registered trademarks of Microsoft Corporation. All other trademarks are the property of their respective owners. Copyright Keysight Technologies 2006 - 2017 All rights reserved.