Can I use multiple M9485A with one controller?
Yes, but there are some limitations. Please refer to below.
- M9485A SFP can’t share same module with multiple instances.
- Modules that are launched on different instances cannot be included in the same chassis.
- The maximum number of chassis available depends on the controller.