Column Control DTX

U3801A/02A IoT Fundamentals Applied Courseware

Data Sheets

Introduction

The Internet of Things (IoT) is the next mega trend that will change the way we live and work, and it is predicted to touch almost every consumer and industrial application. The core technologies that enable the IoT are wireless communication and sensor developments, and ongoing advances in these technologies result in unique challenges.

These challenges include new communications standards, increased sensor integrations and power consumption management. This puts a heavy stress on an IoT device’s design and validation cycle, and designers must constantly innovate to quickly and successfully develop and deploy IoT devices in the market.

The next generation of engineers will play a key role in the development of the IoT, and it is important that students graduate from an undergraduate engineering program prepared for the electronic design, test and measurement challenges needed to be solved in the industry.

To fulfill that goal, education institutes must not only teach students the basics of testing and designing an IoT system, they must provide students with an understanding of the entire IoT ecosystem and also relate these experiences to real-world applications.

With more than 75 years of test and measurement expertise, Keysight Technologies, Inc. is ready to help you to nurture the next generation of IoT-ready professionals.

Keysight’s ready-to-teach U3800 Series IoT applied courseware focuses on teaching practical design and test techniques and is designed to give students the opportunity to work with industry-grade test and measurement instruments in the lab – the same instruments that they would use when they are out in the industry.

There are four IoT applied courseware:

1. IoT Fundamentals – Introduces the fundamentals of IoT. Students who complete this course will have an overview of the IoT’s architecture, technologies and ecosystem.

2. IoT Systems Design – Introduces IoT system design techniques, leveraging embedded systems focusing on specific IoT examples. Students will be able to design and develop an IoT system targeting IoT gateway and sensor network.

3. IoT Wireless Communications – Allows students to develop typical IoT applications with various types of wireless connectivity. Students will be able to perform quick verification and design validation on these IoT applications. This courseware will be available in Fall 2017.

4. IoT Sensors and Power Management – Teaches students how to characterize the power consumption of the IoT device’s on-board controller, sensors and wireless modules. Students will understand the principles of power management and will be able to characterize micro electro-mechanical systems (MEMS) devices. This courseware will be available in Fall 2017.

Each courseware comes with a training kit and teaching slides. The training kit consists of a development kit, IoT sensor device, XBee ZigBee® kit, lab sheets, and problem-based assignments. Students can also use this kit to develop their own projects once they have completed the course.

Courseware Overview

The U3801A/02A IoT Fundamentals applied courseware is a ready-to-teach package focusing on the fundamentals of the Internet of Things. It introduces students to the IoT’s architecture, technologies and ecosystems. The courseware is designed as a resource for lecturers, and consists of teaching slides and a training kit.

  •  Targeted university subject: IoT systems, IoT fundamentals
  •  Targeted year of study: Second to final year undergraduates
  •  Prerequisites(s): Basic programming

Key features and benefits

  •  The IoT Fundamentals applied courseware is designed for a full semester of teaching, and comes with teaching slides and a training kit. Educators can use this complete solution to accelerate the setup of a new IoT-focused course.
  •  The courseware integrates hands-on industry-relevant experiences and real-world applications in IoT design and testing, allowing students learn the design and test techniques practiced by the industry.
  •  The courseware material will be updated yearly for three years at no additional cost. This allows educators and students to keep pace with evolving IoT trends and technologies, which will change rapidly over the next several years.
  •  The IoT development kit is based on a carrier board with Arduino UNO form factor interface and an add-on ZigBee module. Various external sensor devices can be connected to the board, allowing students to implement different types of IoT applications.
  •  The development kit allows students to experiment with wireless local area network (WLAN) 802.11, Bluetooth® Low Energy (LE) and ZigBee wireless connectivity. Due to the kit’s modular design, it can be easily expanded to include other wireless connectivity and sensors.
  •  The development kit provides various test points for troubleshooting, current-drain consumption measurement on sub-circuits, and sensor verification.
  •  The hardware building blocks are visible on the development board.
  •  The development kit is equipped with an Intel Edison compute module that runs on Yocto Linux and is compatible with Intel System Studio IoT Edition, which is an Eclipse-based integrated development environment (IDE). This allows students to compile C/C++ files or to run Python scripts.

Learning outcomes

Students will be able to:

  •  Understand IoT concepts and the various building blocks, applications and ecosystems associated with the IoT
  •  Understand the architecture, standards and connectivity protocols in IoT
  •  Understand the workflow of hardware and software development in IoT from sensors to mobile devices

×

Please have a salesperson contact me.

*Indicates required field

Preferred method of communication? *Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX