About Command Expert
 

Keysight's Command Expert software combines instrument commands, documentation, syntax checking, command execution, and code generation all in one simple interface. Command Expert works with instruments that use Standard Commands for Programmable Instrumentation (SCPI), IVI-C,  or IVI-COM drivers.

Command Expert generates a SCPI.NET driver for each SCPI command set you install, for use in Visual Studio applications.

Command Expert Add-ons let you use Command Expert for easy instrument control in Excel, LabVIEW, MATLAB, Python, SystemVue, VEE, and Visual Studio.
 

What's In Command Expert 1.6 Update 1?

New Development Environment Support

  • LabVIEW 2016
  • MATLAB R2016b

 

What's In Command Expert 1.6?

New Development Environment Support

  • Python 3.5 (32-bit and 64-bit)
  • Visual Studio 2015

New Add-ons and Code Generators

  • New Visual Studio Add-on
  • Python PyVISA code generation for SCPI command sets

Other changes and features

  • Provides a pop out window for the Sequence pane, for dealing with large sequences
  • Adds the ability to Import Commands into an existing sequence file

 

Supported Instruments

To see which SCPI instruments are supported, use the Manage Command Sets dialog box in the Command Expert application, or visit the list of Command Expert command sets.

Command Expert also lets you control instruments using IVI-COM and IVI-C drivers.

 

 Last Updated: December 1, 2016