How do I make the AXIe module show up when there is an empty slot between it and the controller?
If you leave an empty slot between the M9537A controller and an AXIe module, you might not be able to use the AXIe module and an error will show up in Windows Device Manager. Below are ways to clear this issue.
- If you can, do not leave an empty slot between the AXIe module and the M9537A. For example, if you have 2 AXIe modules, put them in slots 2 and 3.
- If you have to have the empty slot, reboot the M9537A from the Start menu without removing power from the AXIe chassis.
- Or from the AXIe chassis Web interface, change the PCIe Upstream connection wait time from 5 seconds to 15 seconds.