Starting Download..
save Save

How do I measure a pulsed RF signal output with a sampling oscilloscope?

There are two possible ways:

  1. Use the PNA/PNA-X to create the pulsed-RF signal using the internal modulator, and use one of the rear-panel pulse output signals to trigger the oscilloscope.
  2. Use two rear-panel pulse output signals. One would trigger an external modulator (with the PNA providing the RF carrier), and one would trigger the oscilloscope.
Was this helpful?


Didn't find what you're looking for?