Eric Bogatin, Signal Integrity Journal Technical Editor
Eric Bogatin, Signal Integrity Journal Technical Editor RSS FeedRSS

Eric Bogatin_new headshot_100

Eric Bogatin is Technical Editor at Signal Integrity Journal and the Dean of the Teledyne LeCroy Signal Integrity Academy. Additionally, he is an Adjunct Professor at the University of Colorado - Boulder in the ECEE Dept. Eric improves the signal to noise ratio by sorting through all of the information available and finding the best quality content to publish on signalintegrityjournal.com.

Best Practices for Connector Models

September 30, 2016

At the recent 2016 IEEE EMC Symposium in Ottawa, I had the opportunity to talk with two of the worlds’ experts on high frequency electrical characterization of interconnects and gained new insight on best practices for connector modeling and measuring.

Heidi Barnes is the ADS application engineering specialist with Keysight Technologies and Jim Nadolny is the Principle SI Engineer for Samtec. Between them, they have more than 40 years’ experience at precision electrical measurement and modeling methods.

 “Everyone asks for models, but they really don’t know what they want or need.” Heidi says. If the application is above about 1 GHz, SPICE based models aren’t very accurate, so the model has to be in the form of an S-parameter behavior model.

It is rare the S-parameter model comes directly from a measurement since the board or cables connecting on either end of the connector has to be exactly the same as what is used in the final customer’s configuration. This means most connector models come from 3D full wave simulations.

“It’s easy to simulate a connector model,” Jim says, “However, it takes a lot of experience and know-how to get it right. To get it right requires attention to material properties, configuration of the return path, excitation port setup and accurately representing the mating PCB stackup ”

It is impossible to accurately separate where the connector ends and the board or cable begins.

Heidi reiterated that, “Due to the variation in the fringe fields, you should only separate one device from another in the middle of a uniform transmission line. You want the fields to become TEM. The length of the uniform transmission lines from the nearest via or pad of the connector should be at least 5x the distance of the field lines to the nearest transmission line ground return.”

Connectors

Figure 1. Close up of a USB 3.1 connector with uniform transmission lines to the edge of the board where the connector model ends. Courtesy of Heidi Barnes, Keysight Technologies.

“Our customers ask for models for connectors, but they may not appreciate the importance of the mating PCB on the resultant performance” Jim says.

This is one of the motivations for Samtec to introduce the idea of the “final inch” more than ten years ago. This highlights the importance of the break out region (BOR) in the board influencing the connector performance. This includes the board level fan out, pad stack and return pin connections. It can influence the overall performance of the connector in a product as much or more than the connector itself.

Samtec, as well as all the high end connector vendors, offer a service to provide a complete model of their connector with the custom board stack and routing provided by the customer. Including the final inch interconnects in the connector model is one of the three types of models Samtec creates.

Their minimalist connector model uses coax port connections to the end of the connector. This model is used to optimize the connector design and is used for rapid-turn internal development. This “Zen” model is often used to extract the three most important figures of merit of a connector, the characteristic impedance, the channel to channel cross talk and the return loss.

When validating the connector models from 3D full wave simulations, Samtec builds a board with minimal board level interconnects to fan into the selected connector pins. This model does not have to match the customer applications. It is optimized for high bandwidth measurement.

In these applications, the connector is embedded in a board with coaxial connectors to interface to a VNA. The board acts as a geometry transformer to go from the coax of the VNA to the board level uniform transmission lines feeding the connector.

“This makes the technology to “de-embed” the connector and its breakout region from the rest of the fixture on either end a critical step when comparing the measurement to the 3D model,” Heidi says. “The Keysight Automatic Fixture Removal (AFR) method is one of the more popular approaches to de-embed devices under test from measurement fixtures.”

You must login or register in order to post a comment.