Highlights:
- 64 GBaud BERT for PAM-4 and NRZ
- Streamlines receiver test setups with highly integrated pattern generator
- Repeatable results with true PAM-4 error detection
- Scalable and upgradeable for future needs
- Extension of M8000 series of BER test solutions
SANTA ROSA, Calif., May 18, 2016
Keysight Technologies, Inc. (NYSE: KEYS) today introduced a M8040A high-performance BERT for testing PAM-4 and NRZ devices that operate up to 64 GBaud. Engineers in validation labs and R&D who characterize receivers on the physical layer for the next generation of data center interconnects will benefit from simplified test setups and repeatable and accurate results.
Today's data center infrastructure is continuously optimized to address bandwidth capacity growth, power, reach and service differentiation. Higher transmission rates, more transmission lanes and new multi-level data formats like PAM-4 address the increased transmission bandwidth demand for the next generation data center interconnects.
The latest revisions of IEEE 802.3 bs and OIF CEI-56G implementation agreements define PAM-4 and NRZ interfaces for electrical chip-to-chip, chip-to-module, backplane connections and optical interfaces for up to 400 Gbit/s bandwidth. R&D and validation labs who need to characterize receivers for data center interconnects with PAM-4 or NRZ data rates up to 64 GBaud are facing new test challenges, such as tighter timing margins, channel loss, non-linearity, level interference and crosstalk effects—making test efficiency and accuracy essential.
"The new 64 GBaud BERT for PAM-4 and NRZ extends our industry leading M8000 series for 400G," said Jürgen Beck, vice president of Keysight's Networks and Data Centers Solutions Business. "With its unique level of integration and scalability we enable R&D and test engineers to master the receiver test challenges for 400G data center interconnects."
The new M8040A is the latest member of the modular AXIe based M8000 series of BER test solutions. It is a highly integrated BERT that supports PAM-4 signals up to 64 GBaud and NRZ signals up to 64 Gbit/s. The pattern generator module provides built-in de-emphasis, jitter injection and an optional second channel. Engineers and designers can select PAM-4 and NRZ in the user interface, eliminating the need for external combiners, cabling and deskew to provide PAM-4 signals. For best signal quality, remote heads reduce the distance to the device under test. The analyzer module provides true PAM-4 error analysis in real-time for long PRBS and QPRBS patterns. This allows proofing even low bit error ratios and symbol error ratios with the required confidence. Users can control the M8040A from a graphical and remote control interface.
More information about the Keysight M8040A 64 GBaud BERT is available at www.keysight.com/find/m8040a.
Images are available at www.keysight.com/find/M8000_images.
U.S. Pricing and Availability
The price of a M8040A BERT starts at $323,000 for a 32 GBaud PAM-4 BERT with one channel, including the M8070A software, and is available now for ordering.
About Keysight in Digital Test
Keysight's solutions for digital applications are driven and supported by Keysight experts who are involved in various international standards committees. Keysight experts are active in the Joint Electronic Devices Engineering Council (JEDEC), PCI Special Interest Group (PCI-SIG®), Video Electronics Standards Association (VESA), Serial ATA International Organization (SATA-IO), USB Implementers Forum (USB-IF), Mobile Industry Processor Interface (MIPI®) Alliance, Ethernet standards (IEEE 802.3), Optical Internetworking Forum (OIF) and many others. Keysight is committed to involvement in standards groups and related workshops, plugfests and seminars to ensure the right test solutions are created to meet customers' evolving needs.
About Keysight in Modular
Keysight provides unrivaled PXI and AXIe performance built on the industry's most accurate measurement science. Keysight helps engineers get to first measurement faster with common measurement software and Keysight Reference Solutions. Keysight has the industry's largest global network of experienced application engineers and metrology-grade calibration centers. Additional information about Keysight's PXI and AXIe modular test and measurement solutions is available at www.keysight.com/find/modular.
Keysight Technologies (NYSE: KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2015. Information about Keysight is available at www.keysight.com.
# # #
PCI-SIG® is a registered trademark of PCI-SIG.
MIPI® service marks and logo marks are owned by MIPI Alliance, Inc. and any use of such marks by Keysight Technologies is under license. Other service marks and trade names are those of their respective owners
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com