=============================================== README.TXT EasyEXPERT for PC =============================================== This document contains the following: * Introduction * System Requirements * Installation Instructions * Before Starting Desktop EasyEXPERT * Other Documents * Known Defects * Software Revision Introduction ============ The EasyEXPERT group+ GUI based characterization software is furnished with the Precision Current- Voltage Analyzer Series to accelerate the current-voltage characterization (IV characterization). It is available on your PC to support efficient and repeatable characterization across the entire process from measurement setup and execution to analysis and data management and so on, using the graphical intuitive user interface and mouse/keyboard operation. Various powerful features of EasyEXPERT group+ allow you to perform the measurement quickly and acquire the result graphically, dramatically improving the productivity of characterization. It has become increasingly important to accelerate the IV characterization, because it is necessary to fully understand the electrical behaviour of devices and materials. This is true no only for semiconductor devices, but also for other devices such as nano-components, photovoltaic cells, optical devices, organic devices, sensors, passive/active discrete components and automotive devices. There is much on-going research into improving these devices to decrease power consumption and lower costs so as to improve the overall performance of the consumer devices in which the devices ultimately reside. NOTE: For more details of the supported instruments and features, refer to the EasyEXPERT group+ technical overview. System Requirements =================== The following is the minimum requirement for executing EasyEXPERT group+ software on an external PC. - Display: XGA 1024x768 (SXGA 1280x1024 recommended) - Hard disk drive: 1 GB free space in the C drive, more than 30 GB free space is recommended for test setup/result data storage. - GPIB interface (for the Online execution mode): - Keysight 82350B/C, 82351B PCI type GPIB interface; highly recommended - Keysight 82357A/B USB type GPIB interface - National Instrument GPIB-USB-HS NOTE: USB GPIB interface might cause serial poll error. See more details in the Data Sheet. - Operating systems: - Windows Vista Business Version SP2 or later (32bit) - Processor: Vista certified PC - Memory: 2 GByte memory - Windows 7 Professional SP1 or later (32bit/64bit) - Processor: Windows 7 certified PC - Memory: 2 GByte memory - Windows 8.1 Professional SP1 or later (32bit/64bit) - Processor: Windows 8.1 certified PC - Memory: 2 GByte memory - Windows 10 Pro or later (32bit/64bit) - Processor: Windows 10 certified PC - Memory: 2 GByte memory- Language: - English (US) or Japanese - Software: - Microsoft .NET Framework 3.5 Service Pack 1 - Keysight IO Libraries Suite 16.2, 16.3, 17.1 update 1 or later (for the Online execution mode) NOTE: For Windows 10, IO Libraries Suite 17.1 update 1 or later is required. NOTE: If all the required software is not installed, install them in the above sequence. For example, if a certain software is not installed, install it and then install all the software that are listed after the software, in the sequence listed above. If you are installing to Windows 8.1/10, you need either the Windows 8.1/10 DVD-ROM or Internet connection to install the .NET 3.5, because by default the .Net 3.5 is not installed on Windows 8.1/10. In this case, refer to the ".NET 3.5 Installation Instruction for Windows 8.1" that is available in the download website. For the IO Libraries Suite, obtain from Keyisight.com website. The other required software are stored in the Prerequisites folder. Note that EasyEXPERT for PC does not support IO Libraries 14.2 or prior versions. Installation Instructions ========================= To install EasyEXPERT group+ onto your computer, follow the procedure below. 1. Insert the EasyEXPERT group+ software CD-ROM into the CD-ROM drive or install the downloaded files to your PC. 2. Double click the index.html file. 3. Click "Install EasyEXPERT for PC" icon and follow the instructions of the setup wizard. 4. Wait for installation to complete, and remove the CD-ROM from the CD-ROM drive. 5. Launch Start EasyEXPERT by selecting from the Start menu or by double clicking the Start EasyEXPERT icon on the desktop. The Start EasyEXPERT window and the Execution Mode dialog box are displayed. 6. In the dialog box, set the execution mode to Online or Offline. 7. If you select the online mode, set the GPIB interface on your computer and the GPIB address of the B150xA or E5260/E5270/4155/4156 connected to your computer via GPIB. NOTE: To optimize the appearances of the EasyEXPERT window, set the Font size to "Normal" on the Display Properties window's Appearance tab. To open the Display Properties, launch "Display" from the Control Panel. Supported instrument and the firmware requirement is as follows. - B150xA - A.04.00 or later - E5260A/E5262A/E5263A/E5270B - B.01.10 or later - 4155B/C, 4156B/C - HOSTC: 03.08 or later - SMUC: 04.08 or later - B2900A Series - 1.0 or later If the firmware revision does not match, open the README file in the "415x Firmware Image" folder on this CD-ROM, and follow the instruction to update the firmware. Before Starting EasyEXPERT for PC ================================== Note the following when starting EasyEXPERT for PC. - When using the offline mode, use the data import/export function to transfer your test setup data files and test result records. - When using the online mode with B150xA, exit EasyEXPERT on the B150xA. The Start EasyEXPERT window (button) must be displayed or be minimized to the Windows task bar on the B150xA screen. - Do not send a control command to B150xA or B2900/E5260/E5270/4155/4156 by using a programming environment except for EasyEXPERT for PC. - Do not send a control command to B150xA or B2900/E5260/E5270/4155/4156 by using the GPIB IO statement in a test definition of EasyEXPERT. Other Documents =============== The following electronic manual is available to use this software. This is stored in the Keysight B150xA Manual CD-ROM. - Keysight B150xA User's Guide - Keysight B150xA Self-paced Training Manual Known Defects ============= There are no known defects in this program. Software Revision ================= A.02.00 April 2006 Initial release. A.02.10 June 2006 Update to add some features and to fix some defects. A.02.11 September 2006 Update to add some features and to fix some defects. A.03.00 June 2007 Update to support 4155/4156 with some additional features and to fix some defects. A.03.10 November 2007 Update to add some features and to fix some defects. A.03.11 July 2008 Update to support Microsoft .NET Framework 2.0 SP1, some additional features and to fix some defects. A.03.20 November 2008 Update to support Windows Vista, new WGFMU module, some additional features and to fix some defects. A.04.00 June 2009 Update to support B1505A with some additional features and to fix some defects. A.04.02 October 2009 Update to fix some defects. A.04.03 January 2010 Update to fix some defects. A.04.10 May 2010 Update to add some features and to fix some defects. A.04.11 December 2010 Update to fix some defects. A.04.20 August 2011 Update to support Windows 7 and to fix some defects. A.04.21 March 2012 Update to fix some defects. A.05.00 June 2012 Update to some features and to fix some defects. A.05.01 September 2012 Update to some features and to fix some defects. A.05.02 November 2012 Update to some features and to fix some defects. A.05.03 January 2013 Update to add some features and to fix some defects. A.05.04 April 2013 Update to fix some defects. A.05.50 May 2013 Update to add some features and to fix some defects. A.05.60 October 2014 Update to add some features and to fix some defects. A.05.61 December 2014 Update to fix some defects. 6.0 June 2015 Update to add some features and to fix some defects. 6.1 Feb 2016 Update to add some features and to fix some defects. Microsoft and Windows are registered trademarks of Microsoft Corporation. All other trademarks are the property of their respective owners. Copyright Keysight Technologies 2006 - 2016 All rights reserved.