Highlights:
- General Test Systems win CMCC OTA test system bid
- Solution integrates Keysight UXM wireless test set
- Can be upgraded to support MIMO OTA
SANTA ROSA, Calif., Jan. 28, 2016
Keysight Technologies, Inc. (NYSE: KEYS) today announced that General Test Systems' (GTS) RayZone-7000 OTA solution, which integrates Keysight Technologies' UXM wireless test set, won the China Mobile Communications Corporation (CMCC) Terminal Test Center's recent bid.
The solution, chosen by CMCC terminal test center in Hangzhou, China, is a GTS RayZone-7000 OTA Test system, which offers 2G/3G/4G SISO test capabilities. This solution can also be upgraded to support the radiated two stage (RTS) and the multi-probe anechoic chamber (MPAC) MIMO OTA measurement methodologies.
The system integrates Keysight's UXM Wireless Test Set. For RTS LTE/LTE-A FDD and TDD, the system exploits the unique and advanced capabilities of the UXM's built in channel emulator. This embedded emulator supports spatial channel models and calibrations essential to the operation of RTS, thus reducing the complexity of the system and enabling developers to evaluate real-world performance of devices.
GTS developed its proprietary RayBond wave-absorbing material for its anechoic chamber, which features high-performance electromagnet wave absorbency, is deformation-proof and humidity-proof, and is environmental friendly.
The UXM is the ideal choice in this application as it supports the mainstream cellular formats, including 4G/3G/2G, Carrier Aggregation, 4x4 MIMO and TM9. The test set enables engineers to stress UE performance, such as VoLTE, battery drain and full rate end-to-end data throughput up to 600Mbps.
More information about Keysight's UXM wireless test set is available at www.keysight.com/find/UXM. High resolution images are available at www.keysight.com/find/UXM_images. Videos demonstrating the UXM's versatile capabilities are available on YouTube. Contact Keysight at www.keysight.com/find/contactus for E7515A UXM pricing and delivery information.
About Keysight in Wireless
From WLAN to LTE-Advanced to the new 5G technologies, Keysight is focused on tackling the toughest design and test problems in the industry with the broadest range of solutions. With the most advanced electronic measurement solutions consisting of powerful software tied to both benchtop and modular hardware, engineers are able to get greater insight into design and test from simulation to R&D, from validation to manufacturing, from conformance to deployment. With experienced engineers in significant roles in cellular and WLAN standards groups and hundreds of application engineers all over the world, Keysight expertise is there to solve customer problems. Additional information is available at www.keysight.com/find/UXM and www.keysight.com/find/cellular. A knowledge library of application notes, CDs and more is available at www.keysight.com/find/cellular-insight.
Keysight Technologies (NYSE: KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2015. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com