Choose a country or area to see content specific to your location
Flyers
Keysight Technologies
E5080A ENA: Code Compatibility Solutions for E5071C and 8753 Network Analyzer Users
Introduction
The Keysight Technologies, Inc. E5080A ENA network analyzer offers the compatibility solutions that help you migrate your E5071C and 8753 network analyzers to the E5080A. The compatibility solutions support the majority of commands and functions used in the S-parameter measurements. You can seamlessly migrate your automatic test equipment (ATE) systems to next generation with minimal efforts, and take advantage of improved performance and measurement speed using the E5080A.
E5071C Code Emulation and State File Conversion Tools
The E5071C compatibility solution consists of two elements—the E5071C code emulation mode and the E5071C state file converter.
E5071C Code Emulation mode
The E5071C Code Emulation mode enables the E5080A to run remote programming codes with E5071C SCPI commands. The command emulation is performed by the firmware in real time. You can start the emulation mode by choosing “5071” in the Code Emulation softkey under the System menu
E5071C state file converter
The state file compatibility is also important because many manufacturing customers save their test settings in the state files. The E5071C state file converter is the application software that converts the E5071C’s state files to the E5080A’s. The state file conversion between two analyzers can be easily done by using a USB memory stick.
8753 Code Emulation Tool
The 8753 Code Translator (CxL) is the application software which runs on the E5080A and emulates the 8753 commands
Unlock Content
Sign up for free
*Indicates required field
Thank you.
Your form has been successfully submitted.
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.