Quick Install - Windows
IC-CAP can be installed on a computer running Windows by downloading the IC-CAP install file from Keysight EEsof EDA website.
Obtain IC-CAP License File
IC-CAP requires a license to run. You can either apply for an Evaluation or a Purchased license. Once the license request is approved, a license file (with .lic extension) is sent as an email attachment. Save this file on your computer at C:\Program Files\Keysight\EEsof_License_Tools\bin\licenses.
Supported Platforms
For details on Supported Platforms, refer to the Supported Platforms section.
System Requirements
The following are Keysight recommended configurations:
CPU | Intel Pentium © 4 or higher, AMD XP 3000 or higher. |
---|---|
Display | High-resolution color only (Super VGA, 1024x768, 15-inch monitor minimum and at least 1280x1024 is required for Extraction packages). |
RAM | Minimum is 2 GB RAM, recommended is 3 GB RAM. Minimum 3 GB RAM is required for Windows 7. |
Acrobat Reader | Acrobat Reader 5.0 or higher to view the PDF files. |
Hard Disk | 1.5 GB for complete installation. |
Compiler | (Only for user-compiled code interface or open measurement interface). C++ and C: Microsoft Visual Studio .NET 2012 Update 2. |
Supported Instrument Interfaces
If you are using IC-CAP with an NI or Keysight GPIB interface, install the interface and its driver according to the instructions provided with the interface.
Description | Part Number |
---|---|
Keysight GPIB PCI card and Keysight IO Libraries | 82350A1/B |
Keysight LAN/GPIB Gateway Interface and Keysight IO Libraries | E5810A2 |
Keysight USB/GPIB converter and Keysight IO Libraries | 82357A1/B |
National Instruments PCMCIA-GPIB card and NI-488.2M drivers | 778034 |
National Instruments PCI-GPIB card and NI-488.2M drivers 3 | 778032 |
- This is a discontinued product.
- Typically, LAN has some impact on speed; therefore, it could be slower than a card.
Keysight IO Libraries can substitute for the NI-488.2M drivers.
For the latest information, refer to this manual on our website at: http://www.keysight.com/find/eesof-docs.
TAMS Inc. will no longer be operating after March 2016, so IC-CAP will no longer support these interfaces. They have worked in the past and we have no reason to think they cannot work, but Keysight will have no resources available to resolve issues that might arise.
Description | Part Number |
---|---|
TAMS L488 GPIB/LAN Interface and Keysight IO Libraries version 14.2 | L488 |
For information on how to configure driver for GPIB interface, refer to the Configuring the Driver for the GPIB Interface section.
Download IC-CAP Installer
Click http://www.keysight.com/find/eesof-iccap-latest-downloads to download the installer.
Install IC-CAP
To install IC-CAP, you must have system administrator privileges. Run the downloaded installer and follow the guided tour to complete the installation.
IC-CAP License Setup
At the end of installation, the License Setup Wizard starts automatically after detecting that you do not have a valid license to start IC-CAP. If you choose to skip the license setup, you can complete the process later by clicking Start > Programs > IC-CAP <release_number> > IC-CAP Tools > IC-CAP <release_number> License Manager.
The License Manager has been introduced in the product releases starting October 2012. It is one-stop shop for all licensing tools. |
Node-locked License
To setup a counted license, select the Add or replace a license file option and follow the guided tour to complete the license setup process. In case of a USB dongle, attach the dongle to the USB port and invoke the License Manager to complete the setup process.
You must have system administrator privileges to setup node-locked licenses (Only) on Windows Vista and Windows 7 machines. |
Floating License
To setup a floating license, select the Add or replace a network license server option and follow the guided tour to complete the license setup process. Consult your license administrator for the network path of the license server.
Launch IC-CAP
To run IC-CAP, go to the Start menu and choose Programs > IC-CAP <release_number> > IC-CAP <release_number> .
See Also
Setting Up Licenses on Windows