Data Sheets
N1085A PAM-4 Measurement Application For 86100D DCA-X Series Oscilloscopes
Introduction
Several industry groups and standards bodies are using, or actively considering using, Pulse Amplitude Modulation 4-Level (PAM-4) technology to jump to the next-generation speed class. PAM-4 signaling enables higher throughput for a given channel bandwidth compared to traditional non-return-to-zero (NRZ) signaling.
Working groups within the Optical Internetworking Forum - Common Electrical Interface (OIF-CEI 4.0) and IEEE 400G Ethernet (P802.3bs) are leveraging many of the PAM-4 measurements outlined in Clause 94 of IEEE Std 802.3bj-2014. Examples of Standards or Implementation Agreements (IA) that propose PAM-4 signaling include:
While the PAM-4 parameters are still in the development stages, companies are moving forward with their PAM-4 development and need measurement tools to help analyze their designs quickly and accurately.
Debug and Verify Your Designs Quickly and Easily
Transform complexity into simplicity
Keysight N1085A PAM-4 measurement software saves engineers time and money by automating PAM-4 “pre-compliance” measurements for standards that have not yet been ratified.
Based on the 86100D DCA-X Series oscilloscope platform, N1085A is an easy-to-use oscilloscope application that:
Select industry-leading hardware
Configure your oscilloscope for single or multi-channel capability. The 86100D DCA-X wide-bandwidth oscilloscope is a flexible solution that provides ultra-low jitter performance (as low as 45 fs rms) together with an extremely low noise acquisition system. For return loss, the N1085A software controls an N1055A TDR module (or an economy or performance network analyzer) and performs S-parameter measurements.
Configure your measurements
Customize parameters that are specific to your setup, such as data rate and attenuation. Use default values or enter your own settings including number of waveforms taken; type of pattern; and whether or not to remove the effects of test cables. Choose Normal mode to test within limits or choose Debug mode to test to your custom limits and adjust other test parameters.
More Features to Further Streamline Your Development
Generate reports
Users and your customers are interested in the performance of your device. Share a report that shows the test conditions, summary of pass/fail, summary of all tests, and details for each test. Many include a test-specific screen shot of the measured parameter.
Control your device or other equipment
The Automation tab enables you to enter commands to control external devices or equipment, and to further sequence your tests or to control timing.
Configure your solution in three ways
The hardware and software architecture provides wide flexibility. The N1085A PAM4 measurement application may be run as follows:
This lets you use your PC for more processing power and other applications, or you can have all measurement capability consolidated into a compact solution. For return loss measurements, the N1085A can control an N1055A TDR or ENA/PNA vector network analyzer to perform measurements automatically.
Oscilloscope compatibility
Keysight offers a wide range of electrical and optical test solutions to address current and emerging communications standards. When testing PAM-4 electrical designs, you may choose a hardware combination that fits your device data rate and other higher rate tests for other standards. Each row shows the recommended configuration of hardware and software to measure the many parameters. The multi-module approach is useful for designers who may already own a plug-in module.
Perform key PAM-4 measurements
PAM-4 signaling includes many new measurements and challenging tests. The list below shows the transmit parameters tested by the N1085A software application.
Ordering instructions
The N1085A PAM-4 measurement software is a transportable license (-xTP) that can be assigned by the user to an 86100D DCA-X mainframe or a user-supplied PC. The transportable nature of the license allows the user to move the license from one instrument (or PC) to another.
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.