SANTA ROSA, Calif., Feb. 17, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today announced the E5080A ENA vector network analyzer (VNA), which offers the industry's best combination of RF measurement performance and speed, enabling a tenfold improvement in test time. The new ENA uses the Keysight PNA- and PXI-Series software architecture, making it easier for engineers to take measurements across multiple Keysight VNAs. The ENA also offers a large color touchscreen display with fast access to basic measurements.
The E5080A sets the new standard in RF component testing for R&D and manufacturing environments. The E5080A offers comprehensive functionalities for measuring active and passive components such as amplifiers, mixers, antennas and cables, including balanced DUTs.
Compared to the popular E5071C ENA, the E5080A offers performance advantages including more than 10 dB wider dynamic range (typically 147 dB) and up to 10 times faster measurement speed in real-world test scenarios. These enhancements improve precision and throughput in the testing of RF components such as filters with deep rejection bands.
Keysight is the first VNA vendor to provide a software platform that spans benchtop and PXI-based VNAs. This universal platform uses the best attributes and capabilities of the ENA and PNA families and delivers familiar functionality across all Keysight VNAs. With the new touch-based GUI capabilities, including tabbed softkeys and drag-and-drop operations, the E5080A streamlines measurement flow and helps engineers get better results in less time.
"The E5080A provides the capability and performance needed to characterize the leading-edge RF components used in 4G and next-generation smartphones, tablets and base transceiver stations," said Akira Nukiyama, vice president and general manager of Keysight's Component Test Division. "With its excellent analog performance, the E5080A enables better design margins in R&D and faster throughput on the production line."
U.S. Pricing and Availability
The E5080A ENA series vector network analyzers are available now worldwide. The analyzer can be configured with two or four ports and frequency coverage from 9 kHz to 4.5, 6.5 or 9GHz. Prices are as follows:
More information is available at www.keysight.com/find/E5080A and high-resolution product photos are available at www.keysight.com/find/E5080A_images. A product video is available at www.keysight.com/find/E5080A_video or on YouTube. A product backgrounder is available at www.keysight.com/find/E5080A_backgrounder.
Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com