Starting Download..
save Save

How do I upgrade my E7515A UXM Wireless Test Set?

Frequency and feature options of the UXM are sold at the time of instrument purchase. These are also available as your testing needs change to upgrade at a later date. The upgrade option details can be found in the tables below. It is advisable that you view each row for the upgrade of interest, select and read any linked items and view the installation note details before purchasing and installing the upgrade. In many cases, a license key will be required to activate the internal hardware upgrades. The license certificate and web access is required to redeem a license key. The upgrade sections are divided into three categories as follows:

  • Internal Hardware Upgrades (Ex. Second Cell or Internal Applications Server)
  • External Hardware Upgrades (Ex. Rackmount Kits)
  • Instrument Software (Ex. Frequency Range, Channel Emulator)


Internal Hardware Upgrades:

Before a hardware upgrade is purchased the following steps should be taken:

  1. View the installation instructions by selecting the "Available" links in the tables below for the desired upgrade option.
  2. Determine from the installation instructions the complexity of the installation and whether you will perform the upgrade yourself or have a Keysight Service Center do it for you.
  3. Review the installation instructions to see what the required adjustments and performance tests are once the upgrade is installed.
  4. Required adjustment and performance verification tests are only offered by a Keysight Service Center.

If an upgrade option is going to be installed by an Keysight Service Center, additional labor charges will apply. Your Keysight field engineer can provide an all inclusive quote for this.

All instrument adjustments are automated and require the use of the Keysight Performance Verification & Adjustment Software.

Some hardware upgrades will require the redemption and installation of a license key file to activate the option. Once a redemption certificate is received the license key file can be redeemed at the Keysight Software License Redemption Website.
 

Option

Description

Order As

eDelivery

Installation
Note

Upgrade
Contents

Minimum
Firmware

Adjustments
Required1
Additional Requirements Incompatible With Installed By Installation Time
E7515A Internal Hardware Option Upgrades
506 Extend Frequency Range to 6 GHz E7515AK-506 Yes No

License
Key

1.2.1.0 After first year No Not applicable Customer within the first year and Service Center recommended after the first year Install=0.5 Hrs
Refer to Infoline for details of the standard calibration on service 
C01 Channel Emulator E7515AK-C01 Yes No License Key 1.2.1.0 No No Not applicable  Customer Install=0.5 Hrs
 
C02 Enhanced downlink channel emulation E7515AK-C02 Yes No License Key 1.5.1.0 No No Not applicable Customer Install=0.5 Hrs
D01 Dual IP device Test E7515AK-D01 Yes No License Key 1.6.1.0 No 2 cell UXM Not applicable Customer Install=0.5 Hrs
L01 Protocol Logging Data Source

E7151AK-L01

Yes Available License Key 1.2.1.0  No No Not applicable Customer Install=0.5 Hrs
RB1 RF Up-down Converter B E7515AU-RB1 No No Hardware
 
1.2.1.0 Yes 1 cell UXM Not applicable Service Center only Install=1.5 Hrs
Refer to Infoline for details of the standard calibration on service 
BB1 Digital Baseband Transceiver B E7515AU-BB1 No No Hardware
 
1.2.1.0 No 1 cell UXM Not applicable Service Center only Install=0.5 Hrs 
S01 Internal Applications Server E7515AU-S01 No Available Hardware 1.2.3.0 No 1 or 2 cell UXM Not applicable Customer Install=0.5 Hrs
S02 Internal 10GbE Application Server E7515AU-S02 No Available Hardware 1.7.x.x  No  1 or 2 cell UXM  S01  Customer Install=0.5 Hrs 

1 While the completion of the recommended adjustments and performance tests for a given option upgrade does verify the functionality of the option, it does not guarantee that the entire instrument meets all published specifications. A full instrument calibration is the only way to guarantee that all instrument specifications are being met.

External Hardware Upgrades:

Option Description Order As eDelivery Installation Note Upgrade Contents Minimum Firmware Adjustments Required1 Additional Requirements Incompatible With Installed By Installation Time
E7515A External Hardware Option Upgrades
 1CP Rackmount and Handle Kit E6640AU-1CP
 
 No  Available  Hardware  None  None  None  1CR  User  Install=1.0 Hrs
 KYB USB Keyboard E6640AU-KYB  No  None  Hardware  None  None  None  None  Not applicable  Not applicable
 MSE USB Mouse E6640AU-MSE   No  None  Hardware  None  None  None  None  Not applicable  Not applicable

Instrument Software Update:

  • The software update package for the UXM Wireless Test Set contains the hardware control panel, the measurement application and all other updates required by the individual measurement assemblies inside the instrument.
  • Keysight recommends updating the instrument software version whenever an internal hardware upgrade or measurement application is installed into the Test Set.
  • The latest revision of the instrument software installer can be found at  Keysight UXM Instrument Software Update

Measurement Applications:
 

  • Measurement Applications require the redemption and installation of a license key file (.lic). Measurement application upgrades are meant to be performed by the customer, and no adjustments or performance verification tests are required.
  • In order to redeem a license key, the end user must have a valid redemption certificate and then go to the Keysight Software License Redemption Website
Was this helpful?


Didn't find what you're looking for?