Keysight Technologies’ PXI VNA Wins Multiple Industry Awards

  
  

Selected as One of the Most Significant Products of 2014

SANTA ROSA, Calif., Jan. 14, 2015

Keysight Technologies, Inc. (NYSE: KEYS) today announced that it has received three awards for its recently introduced M937XA PXI Vector Network Analyzer. The awards include 1) Product of the Year from Electronic Products magazine, 2) Top Products of the Year 2014 from Microwave and RF magazine, and 3) Hot 100 Products of 2014: Test & Measurement from EDN. The awards, selected from thousands of products introduced in 2014, are based on votes from readers and editors.

"This set of awards underscores our position as the world leader in vector network analysis solutions," said Gregg Peters, vice president and general manager of Keysight's Component Test Division. "Our customers used words such as "impressive", "superior" and "amazing" to describe this product. These awards indicate that we offer meaningful choices in price, performance and capability that addresses emerging needs in aerospace, defense, wireless communications and more."

The award winning, one-slot PXI vector network analyzers cover 300 kHz up to 26.5 GHz. The new analyzers offer the best PXI VNA performance on key specifications such as speed, trace noise, stability and dynamic range. This enables the PXI VNAs to perform fast, accurate measurements and reduce the cost-of-test by enabling simultaneous characterization of many devices – two-port or multi-port – using a single PXI chassis.

When space is at a premium, engineers can add full, two-port VNA capability with S-parameters to an existing system that has just one open slot. To address applications such as high-volume device testing and highly complex on-wafer testing, engineers can add a single chassis loaded with up to sixteen PXI VNA modules for use as either multiple two-port VNAs, a single 32-port VNA or any combination in between.

More information is available online at www.keysight.com/find/pxivna. High-resolution product images are available at www.keysight.com/find/PXIVNA_images. A product backgrounder is available at www.keysight.com/find/pxivna_backgrounder. A product video is available at www.keysight.com/find/pxivna_video.

See Keysight's complete offering of PXI and PXIe modular products to learn how they deliver performance, innovation and measurement expertise in the PXI form factor.

See the Frost & Sullivan's Growth excellence Leadership Award in PXI given to then Agilent, now Keysight Technologies.
About Keysight Technologies

Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.

# # #

Contact:

Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith

Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com

Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com