Last updated: October 30, 2014
This document describes the features in the Keysight Technologies cdma2000 Lab Application releases. This document contains the original features, as well as enhancements that have been added over time.
cdma2000 is a registered certification mark of the Telecommunications Industry Association. Used under license.
If you are interested in comparing the key feature differences between the latest releases of each of the cdma2000 Test and Lab Applications, see
cdma2000 Applications Feature Comparison.
To determine if a hardware upgrade is required for your testing needs, please review the hardware requirement information at:
http://www.keysight.com/find/8960upgrades
The features offered in this release are identical to those offered in the G.00.05 Release - November 2013.
This release includes all of the features and functionality present in the E1962B cdma2000 Mobile Test Application B.21.09 Release - May 2013 .
For information on how to use the features that are common to the E6702B, E6702T, and E6702D, see the cdma2000 online user's guide located at:
http://wireless.keysight.com/rfcomms/refdocs/cdma2k/default.html
This release has specific hardware requirements. Test sets with serial number<MY5210 require a HW upgrade to run this release.
To determine if a hardware upgrade is required for this release, please review the hardware requirement information at:
_____________________________________________________________________________________________________
This release includes all of the features and functionality present in the E1962B cdma2000 Mobile Test Application B.21.09 Release - May 2013 .
For information on how to use the features that are common to the E6702B, E6702T, and E6702D, see the cdma2000 online user's guide located at:
http://wireless.keysight.com/rfcomms/refdocs/cdma2k/default.html
This release has specific hardware requirements. Test sets with serial number<MY5210 require a HW upgrade to run this release.
To determine if a hardware upgrade is required for this release, please review the hardware requirement information at:
_____________________________________________________________________________________________________
This release includes all of the features and functionality present in the E1962B cdma2000 Mobile Test Application B.20.14 Release - April 2012 .
For information on how to use the features that are common to the E6702B, E6702T and E6702D, see the cdma2000 online user's guide located at:
http://wireless.keysight.com/rfcomms/refdocs/cdma2k/default.html
This release has specific hardware requirements. Test sets with serial number<MY5210 require a HW upgrade to run this release.
To determine if a hardware upgrade is required for this release, please review the hardware requirement information at:
_____________________________________________________________________________________________________
This is a maintenance release. The feature offered in this release are identical to those offered in the E.01.12 Release - March 2012 .
_____________________________________________________________________________________________________
This release includes all of the features and functionality present in the E1962B cdma2000 Mobile Test Application B.20.14 Release - April 2012 .
For information on how to use the features that are common to the E6702B, E6702T and E6702D, see the cdma2000 online user's guide located at:
http://wireless.keysight.com/rfcomms/refdocs/cdma2k/default.html
This release includes all of the features and functionality present in the E1962B cdma2000 Mobile Test Application B.19.07 Release - March 2011 .
For information on how to use the features that are common to the E6702B, E6702T and E6702D, see the cdma2000 online user's guide located at:
http://wireless.keysight.com/rfcomms/refdocs/cdma2k/default.html
Generator
Info
( F4 in Call Control 2 of 4
), then Code Channel
Parameters
( F2 in
Gen Inf
o).
GPIB commands are CALL[:CELL[1]]:FCHannel[:FORWard]:QOFunction:MIDentifier
, CALL:SCHannel[:FORWard]:QOFunction:MIDentifier
and CALL[:CELL[1]]:OCNSource:QOFunction:MIDentifier
. See QOF, QOF Mask ID and
QOF Set for more information.Teleservice
is set to User
Specified
; for the mobile originated
SMS, allows you to query the current teleservice
ID that is being used. See the GPIB commands
at CALL:SMService:MTERminated:TELeservice:NUMBer
and CALL:SMService:MORiginated:TELeservice:NUMBer?
_____________________________________________________________________________________________________
This release includes all of the features and functionality present in the E1962B cdma2000 Mobile Test Application B.18.12 Release - December 2010 .
For information on how to use the features that are common to the E6702B, E6702T and E6702D, see the cdma2000 online user's guide located at:
http://wireless.keysight.com/rfcomms/refdocs/cdma2k/default.html
Maximum Number
of Alternative SO
and Flexible
RC/SO Negotiation Mode
support the functionality
together. See Setting Cell
Parameters ._____________________________________________________________________________________________________
This release includes all of the features and functionality present in the E1962B cdma2000 Mobile Test Application B.16.12 Release - October 2009 .
For information on how to use the features that are common to the E6702B and E6702T, see the cdma2000 online user's guide located at:
http://wireless.keysight.com/rfcomms/refdocs/cdma2k/default.html
http://www.keysight.com/find/8960upgrades
_____________________________________________________________________________________________________
Summary of GPIB command changes for this release: GPIB Changes for E6702D D.00- January 2010
This release includes all of the features and functionality present in the E1962B cdma2000 Mobile Test Application B.16.12 Release - October 2009 .
For information on how to use the features that are common to the E6702B and E6702T, see the cdma2000 online user's guide located at:
http://wireless.keysight.com/rfcomms/refdocs/cdma2k/default.html
_____________________________________________________________________________________________________
Summary of GPIB command changes for this release: GPIB Changes for E1962B B.16, E6702C C.01- September 2009
This release includes all of the features and functionality present in the E1962B cdma2000 Mobile Test Application B.16.12 Release - October 2009 .
For information on how to use the features that are common to the E6702B and E6702T, see the cdma2000 online user's guide located at:
http://wireless.keysight.com/rfcomms/refdocs/cdma2k/default.html
http://www.keysight.com/find/8960upgrades
_____________________________________________________________________________________________________
Summary of GPIB command changes for this release: GPIB Changes for E6702C C.00- May 2009
This release includes all of the features and functionality present in the E1962B cdma2000 Mobile Test Application B.15.18 Release - May 2009 . The unique features of the E6702B Lab Application are indicated below.
For information on how to use the features that are common to the E6702B and E6702T, see the cdma2000 online user's guide located at:
http://wireless.keysight.com/rfcomms/refdocs/cdma2k/default.html
_____________________________________________________________________________________________________
Summary of GPIB command changes for this release: GPIB Changes for E6702C C.00.07- December 2008
This release includes all of the features and functionality present in the E1962B cdma2000 Mobile Test Application B.14.14 Release - September 2008 . The unique features of the E6702B Lab Application are indicated below.
For information on how to use the features that are common to the E6702B and E6702T, see the cdma2000 online user's guide located at:
http://wireless.keysight.com/rfcomms/refdocs/cdma2k/default.html
The test set is now able to support the following bands, see Cell Band and RF Channel Number .
In
this release the 2 nd
RF Source (Option 002) is required to allow
you to set the RF
Gen Configure
parameter to GPS
, however future releases will not require this
option.
_____________________________________________________________________________________________________
The E6702T can only be loaded onto an E5515C with Special cdma2000 Lab Application Hardware (or a test set with the equivalent hardware upgrades). Loading the E6702T onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.
Note, the Special High Data Rate Hardware required to support the E6702T meets the E6702B measurement parametric specifications in a temperature range of 25 ° C +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.
The features and functionality offered in this special release are identical to those offered in the B.07.14 Release - September 2008 , with the following key exceptions:
For information on how to use these E6702T features, see E6702T User Documentation .
For information on how to use the features that are common to the E6702B and E6702T, see the cdma2000 online user's guide located at:
http://wireless.keysight.com/rfcomms/refdocs/cdma2k/default.php
_____________________________________________________________________________________________________
Summary of GPIB command changes for this release: GPIB Changes for E1962B B.14, E6702B B.07 - September 2008
This release includes all of the features and functionality present in the E1962B cdma2000 Mobile Test Application B.14.14 Release - September 2008 . The unique features of the E6702B Lab Application are indicated below.
For information on how to use the features that are common to the E6702B and E6702T, see the cdma2000 online user's guide located at:
http://wireless.keysight.com/rfcomms/refdocs/cdma2k/default.html
Enhanced Roaming Indicator is added and can be used to check whether the Mobile Station can display a indicator that indicates the roaming condition.
_____________________________________________________________________________________________________
The E6702T can only be loaded onto an E5515C with Special cdma2000 Lab Application Hardware (or a test set with the equivalent hardware upgrades). Loading the E6702T onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.
Note, the Special High Data Rate Hardware required to support the E6702T meets the E6702B measurement parametric specifications in a temperature range of 25 ° C +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.
The features and functionality offered in this special release are identical to those offered in the B.06.08 Release - July 2007 , with the following key exceptions:
For information on how to use these E6702T features, see E6702T User Documentation .
For information on how to use the features that are common to the E6702B and E6702T, see the cdma2000 online user's guide located at:
http://wireless.keysight.com/rfcomms/refdocs/cdma2k/default.php
_____________________________________________________________________________________________________
Summary of GPIB command changes for this release: GPIB Changes for E1962B B.13, E6702B B.06 - July 2007
This release includes all of the features and functionality present in the E1962B cdma2000 Mobile Test Application B.13.08 Release - July 2007 . The unique features of the E6702B Lab Application are indicated below.
For information on how to use the features that are common to the E6702B and E6702T, see the cdma2000 online user's guide located at:
http://wireless.keysight.com/rfcomms/refdocs/cdma2k/default.html
Support Data Source Reset
Data Source Reset functionality provides a way to reset the data source of Loopback Service Option on every even second boundary of CDMA system time. This functionality can cooperate with Multi-Unit Synchronization feature to test two units soft handoff and mobile receiver diversity verification without coherence setting. See Synchronization Parameters Description for details.
_____________________________________________________________________________________________________
This is a maintenance release to resolve known issues. The features offered in this release are identical to those offered in the T.01.17 Special Release (E6702T) - March 2007 .
_____________________________________________________________________________________________________
This is a maintenance release to resolve known issues. The features offered in this release are identical to those offered in the B.05.17 Release - March 2007 .
_____________________________________________________________________________________________________
The functionality present in the T.01.15 special release is identical to that in the T.01.15 special release (see T.01.12 Special Release (E6702T) - December 2006 ).
_____________________________________________________________________________________________________
The functionality present in the B.05.15 release is identical to that in the B.05.12 release (see B.05.12 Release - December 2006 and GPIB Changes for E1962B B.12, E6702B B.05 - December 2006 ).
_____________________________________________________________________________________________________
The E6702T can only be loaded onto an E5515C with Special cdma2000 Lab Application Hardware (or a test set with the equivalent hardware upgrades). Loading the E6702T onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.
Note, the Special High Data Rate Hardware required to support the E6702T meets the E6702B measurement parametric specifications in a temperature range of 25 ° C +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.
The features and functionality offered in this special release are identical to those offered in the B.05.12 Release - December 2006 , with the following key exceptions:
For information on how to use these E6702T features, see E6702T User Documentation .
A downloadable version of the Online User's Guide (CHM Help File) that is specific to this release is available at:
http://www.home.keysight.com/upload/cmc_upload/All/E1962B_B12_E6702B_B05_E6702T_T01_Ref_Guide.chm
_____________________________________________________________________________________________________
The most current documentation for the cdma2000 applications is the Online User's Guide located at:
http://wireless.keysight.com/rfcomms/refdocs/cdma2k/
Summary of GPIB command changes for this release: GPIB Changes for E1962B B.12, E6702B B.05 - December 2006
A downloadable version of the Online User's Guide (CHM Help File) that is specific to this release is available at:
http://www.home.keysight.com/upload/cmc_upload/All/E1962B_B12_E6702B_B05_E6702T_T01_Ref_Guide.chm
AWS Band (Band Class 15) has been added to the list of supported bands. See CALL:BAND and CALL:SETup:BAND:[:SELected] .
The test set can demodulate and decode the forward/reverse supplemental channel in Service Option 33. You can test, verify or develop the forward/reverse data application on forward/reverse link, such as Email, FTP upload, MMS upload, etc. See Packet Data Service Configurations for details.
The Fast Device Tune measurement is now supported on the RF OUT ONLY port, and includes a complete front panel user interface. See How Do I Make a Fast Device Tune Measurement? .
_____________________________________________________________________________________________________
The features and functionality offered in this special release are identical to those offered in the B.04.16 Release - July 2006 .
_____________________________________________________________________________________________________
Summary of GPIB command changes for this release: GPIB Changes for E1962B B.11.06, E6702B B.04.16 - July 2006
This firmware revision includes all features in the E1962B cdma2000 Mobile Test Application B.11.06 Release - July 2006 and E6702B cdma2000 Lab Application B.03.21 Release - January 2006 .
A downloadable version of the Online User's Guide (CHM Help File) that is specific to this release is available at:
http://www.home.keysight.com/upload/cmc_upload/All/E1962B_B11_E6702B_B04_E6702T_T00_Ref_Guide.chm
The HTTP Interface in the test set allows you to configure SMS message parameters and content, send and receive SMS messages using HTTP protocol. The HTTP interface allows SMS Gateways to be configured as if the test set is a Short Message Service Center (SMSC), eliminating the need for custom external software to route messages to the correct test set. This emulation of an SMSC makes it possible to route messages directly from the HTTP output interface of one test set to the HTTP input interface of another test set. Additionally, the HTTP interface also facilitates MMS message transfer to and from a mobile station if used in conjunction with compatible MMSC (Multimedia Message Service Center) software. See HTTP SMS/MMS for details.
A new teleservice CATPT (Card Application Toolkit Protocol Teleservice) is added. See CALL:SMService:MTERminated:TELeservice[:ENUM] for details. (It is also applicable to the existing SMS.)
The message display mode is added to the Mobile-Terminated SMS Parameters. See CALL:SMService:MTERminated:MDMode for details. (It is also applicable to the existing SMS.)
Support for Call Waiting
Call Waiting functionality provides you the awareness of a second calling party call while having a voice connection with calling party 1. It also enables you to put current call on hold and connect to the calling party 2, as well as to switch back from calling party 2 to calling party 1.
_____________________________________________________________________________________________________
The E6702T can only be loaded onto an E5515C with Special cdma2000 Lab Application Hardware (or a test set with the equivalent hardware upgrades). Loading the E6702T onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.
Note, the Special High Data Rate Hardware required to support the E6702T meets the E6702B measurement parametric specifications in a temperature range of 25 ° C +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.
The features and functionality offered in this special release are identical to those offered in the B.03.21 Release - January 2006 , with the following key exceptions:
For information on how to use these E6702T features, see E6702T User Documentation .
_____________________________________________________________________________________________________
Summary of GPIB command changes for this release: GPIB Changes for E1962B B.10, E6702B B.03.10 - December 2005
This firmware revision includes all features in the E1962B cdma2000 Mobile Test Application B.10.11 Release - January 2006 and E6702B cdma2000 Lab Application B.03 Beta Release - August 2005 .
A downloadable version of the Online User's Guide (CHM Help File) that is specific to this release is available at:
http://www.home.keysight.com/upload/cmc_upload/All/E1962B_B10_E6702B_B0310_Ref_Guide.chm
_____________________________________________________________________________________________________
This is a pre-release firmware. A pre-release is early firmware that has not been fully qualified.
A downloadable version of the Online User's Guide (CHM Help File) that is specific to this release is available at:
http://www.home.keysight.com/upload/cmc_upload/All/E1962B_E6702B_Ref_Guide.chm
Summary of GPIB command changes for this release: E1962B and E6702A/B/C/D/E/F/T Applications: GPIB Command Revision Information
This firmware revision includes all features in E1962B CDMA2000 Mobile Test Application B.09.14 Release - April 2005 and following new features unique to the E6702B.
The test set can emulates the base station to allows you to set the CDMA system time parameters that are sent to the mobile station. The mobile station uses them to calculate time-based data applications. The settable system time is also used in multiple test sets synchronization. See Setting CDMA System Time Parameters for details.
The multiple test sets either running the E6702B cdma2000 lab application or the E6706A 1xEV-DO lab application can be synchronized on the CDMA system time. This feature is very useful for Hybrid Mode AT/MS tests. See Performing Multi-Unit Synchronization for details.
Two test sets can simulate a wireless network that supports a IS-2000/IS95 (CDMA) and a IS-856 (1xEV-DO) system to perform the function test of the hybrid mode AT/MS. See Hybrid Mode for details.
_____________________________________________________________________________________________________
Summary of GPIB command changes for this release: E1962B and E6702A/B/C/D/E/F/T Applications: GPIB Command Revision Information
This firmware revision includes all of the new features added in the E1962B B.08.20 Release - December 2004 and the following new features unique to the E6702B:
A downloadable version of the Online User's Guide (CHM Help File) that is specific to this release is available at:
http://www.home.keysight.com/upload/cmc_upload/All/E1962B_B09_E6702B_B02_Ref_Guide.chm
The test set supports two standard FPC mode (000 - Primary 800 and 011 - EIB) and one non-standard FPC mode (Ignore FPC Bits). The FPC functionality is used for the mobile station to control the forward traffic channel power level to achieve the target Frame Error Rate (FER). All of the FPC related information, such as parameter settings, displayed results, operations, etc., can be accessed from the Forward Power Control .
To generate faded forward channel signals with AWGN, the test set must be equipped with a rear panel Digital Bus connecting to an external PC running Baseband Studio software. See Digital Bus Information for details.
When the test set's R-FCH gating mode is enabled and the mobile station supports the gating mode, the mobile station will gate the R-FCH/R-Pilot channel when transmitting at 1/8th data rate. See R-FCH Gating for details.
With these settings, you can evaluate the mobile station's behavior in response to the specified calling party number (CPN) parameters (for example, to see whether the mobile station displays the calling party's number as expected). See Calling Party Number Parameters for details.
This feature provides the capability to specify the frame patterns to be sent on the forward traffic channel. A typical usage for specifying the frame pattern is for forward power control EIB test. See F-FCH Frame Pattern Setup ).
The dormant state is an important advantage of the packet data service offering since it allows the mobile station's natural state to be dormancy, where the mobile station does not utilize any radio resources and has minimal power consumption. The subsequent sessions (when the mobile station comes out of dormancy) can be started without having to re-establish PPP link again and the connection time is faster. See Packet Data Connection Processing States for details.
External
PDSN
Connect
Timeout
,
is
added
to
the
Data
Channel
Parameters
menu.
See
Data
Channel
Parameters
for
details.Minimum
Frame
Count
,
is
added
to
the
Frame
Error
Rate
Setup
menu.
See
FER
Measurement
Parameters
for
details.FER
Requirement
setting
is
extended
from
the
range
of
0.1%
to
15%
to
the
range
of
0.1%
to
30%.Eb/Nt
Limit
,
is
added
to
the
Frame
Error
Rate
Setup
menu
(see
FER
Measurement
Parameters
).
Also,
four
new
measurement
results
(Average
Eb/Nt,
Maximum
Eb/Nt,
Minimum
Eb/Nt
and
Eb/Nt
pass/fail)
are
available.
See
FER
Measurement
Results
Specific
to
Lab
Application
for
details._____________________________________________________________________________________________________
The functionality present in this release is identical to that in the B.01.16 Release - December 2003 .
See 8960 Known Issues for more information
_____________________________________________________________________________________________________
This firmware revision includes all of the new features added in the E1962B B.07.15 release (see B.07.15 release - December 2003 ) and the following new features unique to the E6702B:
_____________________________________________________________________________________________________
This firmware revision includes the radioOne , calibration signal, which was previously available only with the E1962B Test Application, B.06.30 release. See B.06.42 release - June 2003 .
In addition, data rate changes can now be made while maintaining a Service Option 33 (High Speed Packet Data) call. See Packet Data Service Data Rates .
_____________________________________________________________________________________________________
This firmware revision includes all of the new features added in the E1962B cdma2000 Mobile Test Application, B.06.20 release, except for the radioOne , calibration signal. The unique features of E6702A added in this release include:
The data channel provides support for Service Option 33, a high speed packet data service. With this feature, a data enabled wireless device connected to the test set's front panel RF port can exchange IP data packets with a server connected to the test set's rear panel LAN port. Depending on the selected service option and data rate, data can be carried on both the F-FCH (Forward Fundamental Channel) and the F-SCH (Forward Supplemental Channel).
Ping, a utility that provides a simple IP connection check, is also supported.
With this firmware revision, the Graphical Access Probe Power measurement has the added capability to display a sequence of up to 60 access probes. Originally, 20 access probes could be displayed.
The time span can now be adjusted to display access probes measured within a specified time period beginning with the first access probe. The span length can be specified to any value from 5 to 120 seconds.
Two markers provide the added capability to display relative (delta) power levels between any two access probes.
A table below the Graphical Access Probe Power graph displays the absolute power level of each access probe, along with the delta power relative to each previous probe. The elapsed (delta) time period between the first access probe and each subsequent probe is also displayed. This table can be scrolled to display any portion of the access probe sequence.
The E6582A Wireless Protocol Advisor is now capable of logging the following:
_____________________________________________________________________________________________________
These are the original features of the E6702A. This firmware release includes all of the features of the E1962B cdma2000 Mobile Test Application, B.04 release and the following features unique to the E6702A.
With the E6582A Wireless Protocol Advisor running on an external PC connected to the test set protocol messages can be logged, filtered, decoded, and saved to file to provide detailed information regarding signaling between the test set and a cdma2000 device. Timestamping of messages and identification of specified signaling events allows analysis of the timing and nature of signaling events.
The graphical access probe power measurement consists of measuring a series of channel power measurements triggered by a rise in RF power detected on the test set's RF input. This measurement is performed with the test set's call limit mode feature turned on. By inhibiting the connection of a call, the cdma2000 device transmits its maximum number of access probes.
Each measurement is displayed in a bar graph with a maximum of 20 access probes displayed at one time.
The FER (Frame Error Rate) measurement includes three new measurement results provided to identify the types of errors counted by this measurement. The three types of errors now identified are:
Soft or Softer handoffs can now be performed because of the addition of another simulated cell (base station). The second cell provides pilot, fundamental, and OCNS channels with settable power levels on the pilot and fundamental channels and settable Walsh codes on the fundamental and OCNS channels. Pilot strength levels are displayed in dB and in units specified in test standards that express power in -0.5 dB increments relative to total cell power.
In addition, a timing delay feature has been introduced that delays the cell 2 timing relative to cell 1 by up to 16 PN chips (13.02 microseconds).
All parameters needed to control pilot detection thresholds are provided in the soft handoff parameters setup.
A softkey has also been added that sends the Pilot Measurement Request Order message to the mobile station, allowing the immediate retrieval of pilot strength and status information at any time during a call, regardless of whether a soft handoff is on or off. Timestamping of pilot strength requests and reports is displayed in a table along with current status information.