Last updated: December 30, 2014
This document describes features and functionality that are part of the Keysight Technologies GSM/GPRS_W-CDMA fast switching lab applications. This document contains the original features, as well as enhancements that have been added over time. For a description of the fast switching application (such as license information, etc.), see Fast Switching Description .
To determine if a hardware upgrade is required for your testing needs, please review the hardware requirement information at:
http://www.keysight.com/find/8960upgrades
Select the appropriate link below to view the required release:
This is a maintenance release. This release has the equivalent features of the following lab applications:
This release updates the E6785J fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below.
This release has the equivalent features of the following lab applications:This is a subscription release of the E6785J application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.
You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
This release has the equivalent features of the following lab applications:
This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:
http://www.keysight.com/find/wlcontract
This release has specific hardware requirements. Test sets with serial number<MY5210 require a HW upgrade to run this release.
To determine if a hardware upgrade is required for this release, please review the hardware requirement information at:
http://www.keysight.com/find/8960upgrades
_____________________________________________________________________________________________________
This release updates the E6785I fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below.
This release has the equivalent features of the following lab applications:
You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this release. Contact your Keysight Sales Representative for more information.
This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:
http://www.keysight.com/find/wlcontract
This release has specific hardware requirements. Test sets with serial number<MY5210 require a HW upgrade to run this release.
To determine if a hardware upgrade is required for this release, please review the hardware requirement information at:
http://www.keysight.com/find/8960upgrades
_____________________________________________________________________________________________________
This is a subscription release of the E6785I application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.
You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
This release has the equivalent features of the following lab applications:
This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:
http://www.keysight.com/find/wlcontract
This release has specific hardware requirements. Test sets with serial number<MY5210 require a HW upgrade to run this release.
To determine if a hardware upgrade is required for this release, please review the hardware requirement information at:
http://www.keysight.com/find/8960upgrades
_____________________________________________________________________________________________________
This is a maintenance release. The features offered in this release are identical to those offered in the H.01.13 Release - March 2012
This release updates the E6785H fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below.
This release has the equivalent features of the following lab applications:
You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this release. Contact your Keysight Sales Representative for more information.
This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:
http://www.keysight.com/find/wlcontract
This release has specific hardware requirements. Test sets with serial number<MY5210 require a HW upgrade to run this release.
To determine if a hardware upgrade is required for this release, please review the hardware requirement information at:
http://www.keysight.com/find/8960upgrades
_____________________________________________________________________________________________________
This is a subscription release of the E6785H application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.
You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
This release has the equivalent features of the following lab applications:
This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:
http://www.keysight.com/find/wlcontract
http://www.keysight.com/find/8960upgrades
_____________________________________________________________________________________________________
This release updates the E6785G fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below.
This release has the equivalent features of the following lab applications:
You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:
http://www.keysight.com/find/wlcontract
http://www.keysight.com/find/8960upgrades
_____________________________________________________________________________________________________
This is a subscription release of the E6785G application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.
You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
This release has the equivalent features of the following lab applications:
This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:
http://www.keysight.com/find/wlcontract
http://www.keysight.com/find/8960upgrades
_____________________________________________________________________________________________________
This is a subscription release of the E6785G application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.
You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
This release has the equivalent features of the following lab applications:
This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:
http://www.keysight.com/find/wlcontract
http://www.keysight.com/find/8960upgrades
_____________________________________________________________________________________________________
This release updates the E6785F fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below.
This release has the equivalent features of the following lab applications:
You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:
http://www.keysight.com/find/wlcontract
http://www.keysight.com/find/8960upgrades
_____________________________________________________________________________________________________
This is a subscription release of the E6785F application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.
You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
This release has the equivalent features of the following lab applications:
This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:
http://www.keysight.com/find/wlcontract
http://www.keysight.com/find/8960upgrades
_____________________________________________________________________________________________________
This is a subscription release of the E6785F application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.
You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
This release has the equivalent features of the following lab applications:
This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:
http://www.keysight.com/find/wlcontract
http://www.keysight.com/find/8960upgrades
_____________________________________________________________________________________________________
This is a subscription release of the E6785U application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.
You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, cdma2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
The E6785U can only be loaded onto an E5515C with Special High Data Rate Hardware (or a test set with the equivalent hardware upgrades). Loading the E6785U onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.
Note, the Special High Data Rate Hardware required to support the E6785U meets the E6785D measurement parametric specifications in a temperature range of 25 +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.
This release has the equivalent features of the following lab applications:
_____________________________________________________________________________________________________
This is a maintenance release to resolve the known issues detailed in the previous release. The features offered in this release are otherwise identical to those offered in the E.01.14 Release - September 2008 , with the following exception:
This release is available for download at the Lab Application Annual Contract site: www.keysight.com/find/wlcontract.
This release has the equivalent features of the following lab applications:
_____________________________________________________________________________________________________
This release updates the E6785E fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below.
This release has the equivalent features of the following lab applications:
http://www.keysight.com/find/8960upgrades
_____________________________________________________________________________________________________
This is a maintenance release to resolve known issues. The features offered in this release are identical to those offered in the U.00.37 Special Release - May 2008 Release.
This release has the equivalent features of the following lab applications:
http://www.keysight.com/find/8960upgrades
_____________________________________________________________________________________________________
This is a maintenance release to resolve known issues. The features offered in this release are identical to those offered in the E.00.39 Subscription Release - May 2008 Release.
This release has the equivalent features of the following lab applications:
http://www.keysight.com/find/8960upgrades
_____________________________________________________________________________________________________
This is a subscription release of the E6785U application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.
You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, cdma2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
The E6785U can only be loaded onto an E5515C with Special High Data Rate Hardware (or a test set with the equivalent hardware upgrades). Loading the E6785U onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.
Note, the Special High Data Rate Hardware required to support the E6785U meets the E6785D measurement parametric specifications in a temperature range of 25 +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.
This release has the equivalent features of the following lab applications:
This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:
This is a subscription release of the E6785E application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.
You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, cdma2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
This release has the equivalent features of the following lab applications:
This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:
This is a subscription release of the E6785U application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.
You must have current GSM/GPRS/EGPRS and W-CDMA/HSPA Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
The E6785U can only be loaded onto an E5515C with Special High Data Rate Hardware (or a test set with the equivalent hardware upgrades). Loading the E6785U onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.
Note, the Special High Data Rate Hardware required to support the E6785U meets the E6785D measurement parametric specifications in a temperature range of 25 +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.
This release has the equivalent features of the following lab applications:
This is a subscription release of the E6785E application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.
You must have current GSM/GPRS/EGPRS and W-CDMA/HSPA Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
This release has the equivalent features of the following lab applications:
The E6785T can only be loaded onto an E5515C with Special High Data Rate Hardware (or a test set with the equivalent hardware upgrades). Loading the E6785T onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.
Note, the Special High Data Rate Hardware required to support the E6785T meets the E6785D measurement parametric specifications in a temperature range of 25 +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.
This release has the equivalent features of the following lab applications:
This release updates the E6785D GSM/GPRS_W-CDMA fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below. This release has the equivalent features of the following lab applications:
This is a subscription release of the E6785E application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.
You must have current GSM/GPRS/EGPRS and W-CDMA/HSDPA Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
This is a maintenance release to resolve known issues. The features offered in this release are identical to those offered in the E.00.13 Subscription Release - April 2007 Release.
_____________________________________________________________________________________________________
This is a subscription release of the E6785U application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.
You must have current GSM/GPRS/EGPRS and W-CDMA/HSDPA Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
The E6785U can only be loaded onto an E5515C with Special High Data Rate Hardware (or a test set with the equivalent hardware upgrades). Loading the E6785U onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.
Note, the Special High Data Rate Hardware required to support the E6785U meets the E6785D measurement parametric specifications in a temperature range of 25 +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.
This release has the equivalent features of the following lab applications:
This is a subscription release of the E6785E application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.
You must have current GSM/GPRS/EGPRS and W-CDMA/HSDPA Lab Application Annual Contracts to obtain this subscription release. Contact your Keysight Sales Representative for more information.
This release has the equivalent features of the following labapplications:
The E6785T can only be loaded onto an E5515C with Special High Data Rate Hardware (or a test set with the equivalent hardware upgrades). Loading the E6785T onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.
Note, the Special High Data Rate Hardware required to support the E6785T meets the E6785D measurement parametric specifications in a temperature range of 25 +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.
This is a maintenance release to resolve known issues. The features offered in this release are identical to those offered in the T.01.12 Special Release - December 2006 .
This is a maintenance release to resolve known issues. The features offered in this release are identical to those offered in the D.01.13 Release - December 2006 .
The E6785T can only be loaded onto an E5515C with Special High Data Rate Hardware (or a test set with the equivalent hardware upgrades). Loading the E6785T onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.
Note, the Special High Data Rate Hardware required to support the E6785T meets the E6785D measurement parametric specifications in a temperature range of 25 +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.
This release has the equivalent features of the following lab applications:
This release updates the E6785D GSM/GPRS_W-CDMA fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below. This release has the equivalent features of the following lab applications:
The E6785T can only be loaded onto an E5515C with Special High Data Rate Hardware (or a test set with the equivalent hardware upgrades). Loading the E6785T onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.
Note, the Special High Data Rate Hardware required to support the E6785T meets the E6785D measurement parametric specifications in a temperature range of 25 +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.
This release has the equivalent features of the following lab applications:
This is a pre-release of the E6785D application. In order to provide early access to new features, this pre-release has not been fully qualified.
You must have current E6720A Option 001 and 003 Lab Application Annual Upgrade Contracts to obtain this pre-release. Contact your Keysight Sales Representative for more information.This release has the equivalent features of the following lab applications:
This release updates the E6785C GSM/GPRS_W-CDMA fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below. This release has the equivalent features of the following lab applications:
This release updates the E6785C GSM/GPRS_W-CDMA fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below. This release has the equivalent features of the following lab applications:
This release introduces the E6785C GSM/GPRS_W-CDMA fast switching lab application with the equivalent features of the following lab applications and application revisions:
For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.
This release introduces the E6785C GSM/GPRS_W-CDMA fast switching lab application with the equivalent features of the following lab applications and application revisions:
For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.
This release introduces the E6785C GSM/GPRS_W-CDMA fast switching lab application with the equivalent features of the following lab applications and application revisions:
For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.
This release updates the E6785B GSM/GPRS_W-CDMA fast switching lab application with the equivalent features of the following lab applications and application revisions:
For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.
This release updates the E6785B GSM/GPRS_W-CDMA fast switching lab application with the equivalent features of the following lab applications and application revisions:
For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.
This release updates the E6785B GSM/GPRS_W-CDMA fast switching lab application with the equivalent features of the following lab applications and application revisions:
For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.
This release updates the E6785A GSM/GPRS_W-CDMA fast switching lab application with the equivalent features of the following lab applications and application revisions:
For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.
This is the initial release of the E6785A GSM/GPRS_W-CDMA fast switching lab application. This release has the equivalent features of the following lab applications and application revisions:
For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.
This is the initial release of the E6785A GSM/GPRS_W-CDMA fast switching lab application. This release has the equivalent features of the following lab applications and application revisions:
For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.