If I have N9051A Pulse Measurement Software, how do I upgrade to N9051B?
Order N9051B Option A2B to receive a user-installed software license, which causes any existing N9051A licenses to be recognized as an N9051B license. The 2FP license is required, while all others are optional and independent of each other.
Important: N9051B runs only on the CPU inside an X-Series signal analyzer (it does not run on an external PC). The CPU must be 64-bit, and the Operating System must be Windows 7.
To check your instrument, press System >> Show >> System and find the following:
- If the Computer System is Windows 7, then it already has a 64-bit CPU; your instrument is ready for N9051B.
- If the Computer System is Windows XP, but the CPU is identified as PC4 or PC5, then you need a software only upgrade to Windows 7, see N9094AK Option W7X for details.
-
If the CPU is identified as PC3 or lower, then your instrument CPU hardware must be upgraded. See N9094AK Option PC4 for details.