How does the N9051B Pulse Measurement Software GUI work?
The GUI is standard MS Windows type: pull-down menus, dialogs, on-screen buttons, etc. A USB mouse and keyboard are required. The PC-standard keys of the X-Series signal analyzer front panel are recognized: numbers (digits 0-9, decimal point, minus, BkSp); plus Enter, Select, Escape, Ctrl, Alt, Del, and Tab; and the Mode key.
The Mode key can be used to launch “Pulse”. When the N9051B is the active app, pressing the Mode key will shut it down and return the user to the last X-Series signal analyzer application previously running. If you Exit or close the N9051B window, the IQ Analyzer app will be active (and in Single).
In the N9040B UXA signal analyzer, with multi-touch GUI, the Mode mechanism is incompatible. However, the N9051B can be “pinned” to the Start menu for easy access.