Starting Download..
save Save

What are the similarities and differences in the N9040B UXA Signal Analyzer when it comes to Real-Time Spectrum Analysis?

 

X-Series Real-Time Similarities Real-Time Differences in the N9040B UXA Signal Analyzer
Update Rate Real-Time Bandwidth on N9040B is ~510 MHz. 
Note:  In Multi-Mode with spectrum and PvT running at the same time, the Real-Time bandwidth will be 255 MHz compared to the N9030A PXA Signal Analyzer, which has a Real-Time bandwidth of 160 MHz and does not offer Multi-Mode.
Triggers including Time-Qualified Trigger (TRT) Minimum signal duration on the N9040B UXA Signal Analyzer for 100% Probability of Intercept (POI) is 3.33 ns for signals with 60 dB Signal-to-Noise ratio.  For 100% POI with full amplitude accuracy the minimum signal duration is 3.517 us in 255 MHz BW and 510 MHz BW.  The N9030A PXA Signal Analyzer has a 100% POI specification of 3.57 us in a 160 MHz BW.
At the first launch, the N9040B UXA RTSA features will be similar to what is currently available in the N9030A PXA and N9020A MXA RTSA mode  
FFT Rate (~300,000 FFT's/sec)  
Was this helpful?


Didn't find what you're looking for?