What will be the maximum SA-mode RBW setting in the N9040B UXA signal analyzer?
The maximum RBW setting in SA-mode is normally 8 MHz except for two exceptions:
a) The Burst Power measurement allows a maximum RBW equivalent to the maximum digitizing bandwidth of the instrument.
b) The Fast Power (FP2) option allows bandwidths up to 40 MHz.
RBWs greater than 8 MHz are also available using other measurements applications that perform FFTs of the IQ data from the instrument’s digitizers. Therefore when using the 89600 VSA software, IQ Analyzer Spectrum Measurement, and Real Time Spectrum Analyzer (RTSA), you can view RBWs greater than 8 MHz.