Can I use a Windows 7 PC to upgrade my PSA Series Spectrum Analyzer?
The program for updating the PSA Series Spectrum Analyzer firmware from a PC was designed to be used for Windows XP. Through using the Windows XP Mode from within Windows 7, it is possible to use a Windows 7 PC to perform the firmware update. Please see the instructions below.
Instructions for running PSA Firmware Update Program in Windows 7