SANTA CLARA, Calif., July 28, 2014
Agilent Technologies Inc. (NYSE: A) today announced that the Modelithics COMPLETE Library of RF and microwave component model libraries is available free of charge for six months to Genesys 2014 users new to Modelithics.
First made available to Genesys users in 2003, the Modelithics COMPLETE Library contains over 10,000 RF/microwave components with accurate nonlinear models for active devices and highly scalable linear models for passive component families. Each model is extracted from a standardized set of highly accurate measurements and carefully documented with individual model data sheets to provide designers with exceptional simulation accuracy and design flexibility when using Genesys 2014.
The Modelithics COMPLETE Library contains Global Models that represent entire RLC component families as compact models with layout attributes, pad de-embedding capability, and offer scaling of part-value, substrate type and thickness, and solder pad geometries. These advanced models ensure that correct physical geometries are available to the Genesys Momentum electromagnetic (EM) simulator for designers to achieve the best possible accuracy from circuit-EM co-simulation of the RF board prior to signing off on hardware fabrication.
Using the Modelithics COMPLETE Library, Genesys 2014 users can now design and realize their products faster and easier with accurate models of popular vendor parts. Easily accessible in the Genesys 2014 schematic and layout design environments, the libraries enable designers to compare the performance, size and ease-of-realization of deploying different vendor parts in their designs so that production-ready circuit or system designs can be finalized in a single pass.
"Accurate models are critical to achieving excellent simulation-based design success," said Larry Dunleavy, president of Modelithics. "In recognition of this need, we are pleased to work with Agilent to make our Modelithics COMPLETE Library available to those Genesys users who have yet to experience the difference our accurate models can make in improving design success and productivity while using Agilent Genesys."
"Our Genesys 2014 customers will definitely appreciate the availability of the Modelithics COMPLETE Library, especially given the high quality of their models," said How-Siang Yap, product planning and marketing manager for Agilent's Genesys software. "Over the years, RF designers worldwide have voiced their desire for access to these models. The six-month promotion now gives our customers access to the best accuracy in the most affordable RF simulation software in the industry."
U.S. Pricing and Availability
Agilent's Genesys 2014 software is now available with pricing starting at $4,000. The free, six-month promotion of the Modelithics COMPLETE library runs throughout 2014 and is available to all Genesys users who complete a simulation modeling needs survey at www.surveymonkey.com/s/Genesys2014_Modelitics-Survey.
More information about the 2014 release of the Genesys RF and microwave design software is available at www.agilent.com/find/eesof-genesys2014. Images of the software are available at www.agilent.com/find/Genesys2014_images.
About Genesys 2014
Genesys 2014 is the latest release of Genesys, Agilent's industry-leading, affordable RF simulation and synthesis software. Designed for circuit and system designers, the software features breakthrough modulated RF analysis as well as enhancements to its powerful, custom-filter direct synthesis technology. Using Genesys 2014, designers can simulate digitally modulated RF signals, like those found in today's defense and consumer wireless applications, as easily as they do traditional analog RF signals.
About Agilent EEsof EDA Software
Agilent EEsof EDA is the leading supplier of electronic design automation software for microwave, RF, high-frequency, high-speed digital, RF system, electronic system level, circuit, 3-D electromagnetic, physical design and device-modeling applications. More information is available at www.agilent.com/find/eesof.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@agilent.com
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@agilent.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@agilent.com