Starting Download..
save Save

How to Find Your Host ID

For licensed applications that are used with the Logic and Protocol Analyzer application software, the Host ID can be found in the Activation tab when you select Help > Software Licensing... (see below).

Software Licensing dialog box, Activation tab

For the following products, the application software and access to the licensing host ID may be slightly different.

  • E5910A Serial Link Optimizer
    • Launch the Serial Link Optimizer software instead of the Logic and Protocol Analyzer application software. The Host ID can be found in the Activation tab of the dialog that is displayed when you select Help > Software Licensing...
    • (If prompted to enter a Serial Number during the redemption process, leave this field blank.)
  • N5998U-001 Upgrade for MHL compliance test
    • Launch the HDMI software application instead of the Logic and Protocol Analyzer application software.
    • Click on the Software Licensing button.
    • The Host ID can be found in the Activation tab.
  • N5998U-DBG Debug Exporter for HDMI
    • In the HDMI Evaluator application, click the Software Licensing... button at the bottom of the application.
    • The Host ID can be found in the Activation tab.
  • N5310U-FCN PCIe Flow Control Analysis Package
    • Launch the Keysight PCIe Analysis software application instead of the Logic and Protocol Analyzer application software.
    • Click on the menu option File > Post Processing Software Packages
    • The Host ID can be found in the Activation tab.
Was this helpful?


Didn't find what you're looking for?