Mwrf 1238 20eteaser 0

System-Level Modelers Race The Design Cycle

April 2, 2014
As system complexity increases, developing a system level model from a project’s start to finish may be the key to a more optimal design. Proper system modeling practices could even prevent costly rework and redesign by revealing design issues before implementation.
Download this article in .PDF format
This file type includes high resolution graphics and schematics when applicable.

The complexity of RF systems is increasing for almost every application. The addition of digital, analog, and RF components, which are critical to the operation of most modern devices, necessitates multi-domain interactions. Yet the interfaces between these different domains are often difficult to describe and analyze in an accurate and timely way. With more tightly integrated and domain-interdependent functions, the barriers between the domains also are breaking down. To effectively model the operational behavior of such systems, the fast-paced RF industry may benefit from multi-domain, system-level modeling tools that can follow a design from conception to implementation.

Related Articles
Millimeter-Wave Technology Prepares For A Wealth Of Applications
Satellites Prove Key To Search
Multifunction Test Sets Target Wireless Devices

By definition, system-level modeling is the functional block-level analysis of a system. There are levels of abstraction to consider when modeling a system. Micro-system-level modeling, such as transistor-level modeling, analyzes the interactions among the individual transistors based upon detailed device models. Conversely, macro-system-level modeling involves the interaction between a device and the much larger environment in which the device may operate. Different considerations exist at various levels of abstraction. 

Frank Ditore, product marketing manager for Agilent Technologies, shares an anecdote: “There is something that we joke around about on our team with system-level design or system-level modeling. It’s that the system is always one level higher than the person you are talking to.” The goal of a system architect is to choose a level of abstraction that can benefit a device’s design process while avoiding the time- and computationally intensive simulation of a too-inclusive system. For a system-level architect, a scalable modeling tool with methods of analysis for each domain would enable more efficient and accurate designs.

Until recently, office productivity tools like Microsoft Excel were the mainstay of the system architect. Spreadsheet-style tools provide a high level of flexibility and a mathematically open and definable environment. Yet spreadsheet tools often fall down when it comes to the effective incorporation of nonlinear effects and multi-domain modeling. Ditore elaborates, “If you look at a filter as a mathematical representation, it is a polynomial. I can model that in a spreadsheet. But if I need to implement that in a DSP or FPGA, it becomes a fixed point or Z-domain representation of that polynomial. If my tool can’t allow me to model in that domain very quickly, that tool becomes less effective.” Because the interfaces between various domains are often hard to detail mathematically, tools that can account for these issues may be best suited to enabling the latest designs.

1. Many system-modeling tools have the capability to support a multi-window interface to capture key aspects of a system and make them readily available to the system architect.

As RF systems are incorporated into more devices, specific tools for RF system-level modeling or RF-capable add-ons for EDA tools are becoming more available.  Modern tools for system-level modeling are often integrated design suites, which allow for the functional block-level analysis of complex systems. Such software includes The Mathworks MATLAB/Simulink/SimRF, Agilent SystemVue, CST Design Studio, and AWR Visual System Simulator (VSS; Figs. 1 and 2).

2. Modeling complex modulation schemes, such as LTE-Advanced, is a major challenge without advanced tools that integrate block-level schematics, parametric analysis, and equation-driven solutions.

An example of the recent advances in technology and industry collaboration is the development of the AD9364, a software-defined-radio (SDR) prototype module from Analog Devices. In this collaboration with The Mathworks, a fully integrated SDR was modeled—in detail—within the MATLAB, SimuLink, and SimRF environments. Reportedly, the model turned out to be highly consistent with the behavior models developed to enhance the prototyping platform. Such models can then be analyzed with the full capability of relevant MATLAB toolboxes and user-defined code.

The controls of the modeled and practical SDRs are supposedly the same, which could save significant time during product design. Another aspect of the prototyping system is that environmental and channel models can be imported into the simulation. This aspect adds another layer of model detail. It also could aid in preparing the design for market. In addition, an early prototype with a computerized test system could be deployed in real-world environments to confirm radio functions that the device is meant to perform. Other organizations, in contrast, would have to develop a custom system-level-modeling structure to enhance their design flow in such a way.

RF Integration, for example, has developed its own system-level-modeling processes known as the System Accelerator Tool (SAX). In discussing the effective use of system-level-modeling tools, Finbarr McGrath, the firm’s chief technologist, comments, “In the best case, it might save you a design cycle. What it certainly does is give you a much higher-quality design and a much better-understood design.” 

This design-enhancing process usually begins with an interpretation of customer specifications. Those specifications are broken down into individual block performance parameters. A system-level-modeling tool is used to cascade the system blocks into a functional model, in which early analysis is performed. Once the block-level definitions are refined, the optimized block parameters are given to the designers.

Using the system model to predict the system component specifications, the designers complete the internal block designs. The process of refining the block-level models with detailed component-level analysis is iterative. When the system blocks are adequately defined, the block performance metrics are fed into the SAX environment. If needed, the overall system is adjusted to account for the enhanced block-level information. McGrath notes, “This process partitions the design in such a way that the block-level model is contained and precise. The design engineer doesn’t have moving specifications, so changes come back to them less often. It also helps to break the chip down in this way early on, as you get a good idea of how you want to test it.”

If performed well, this type of process could prevent the over-designing of systems and enable much faster design-cycle turnaround. Ideally, the same test methods used with the software also would be used to test the physical device. In that case, troubleshooting, error correction, and design refinement could be dramatically decreased.

A critical step in this process is the description of the block-level parameters. As stated by John Broderick, director of systems engineering for RF integration, “Sometimes, we come up with how good a parameter needs to be from experience or estimates. ..we have to build off those behavior modules.” John further explains that depending upon the tool used, simulating the diverse blocks could be a complex or canned solution. Often, these simulation complexities occur when different components are better defined with time, frequency, fixed-point, or floating-point methods of simulation.

Download this article in .PDF format
This file type includes high resolution graphics and schematics when applicable.

Multi-Domain Considerations

Download this article in .PDF format
This file type includes high resolution graphics and schematics when applicable.

Many—if not most—RF systems incorporate multi-domain designs. To effectively model such a system, the different domains could be handled within the same platform. This could prevent time-intensive and potentially error-prone interfacing caused by multiple tool use and custom generation. Ditore shares, “The best way to solve this is by providing different methods of computation that are well integrated. So you could take a fixed-point model, floating model, time-domain RF model, and frequency-domain RF model and combine them all together into one simulation.”

System-level-modeling tools, such as SystemVue, provide different methods of computation to allow different computation models to run efficiently. The ability to neatly interface the different computation methods enables simulations of an entire system to be performed more rapidly than single methods of computation. This class of tools offers frequency- and time-domain computation for both analog and RF. It also provides floating- and fixed-point methods for the digital domain.

With this approach, the method of computation can be tailored to the type of model that is optimal for each individual block within the system. Ditore shares an analog/RF example: To model an amplifier that has a gain and noise figure as well as input and output impedance matching, a frequency-domain simulation would be adequate in terms of speed. Yet a time-domain envelope simulator could be a viable option—if it was not critical to model the impedance matching  and only the gain and noise figures. The time-domain simulation would run faster with the tradeoff of losing the impedance-matching resolution.

For another example, Ditore pointed to a digital representation using a digital-signal-processing (DSP) finite-impulse-response (FIR) filter. A floating-point simulation would produce the FIR filter coefficients. If finite precision is desired, a set number of bits of resolution could be determined for each coefficient. Using a floating-point simulation with 10 bits of resolution for the coefficients—and using 2’s complement format for numeric precision—it may not be possible to run such a system in a reasonable amount of time. A fixed-point simulation could potentially run the same DSP FIR-filter model at a higher rate.

3. Co-site analysis is becoming a more critical step in system-level analysis, as a variety of antennas is being incorporated into almost every platform.

Beyond the system-level-modeling tools that enhance the design flow from the block level, the design of robust devices can be aided by tools that account for environmental factors and other RF systems. For example, RF co-site analysis predicts the interactions between various antenna and radio systems (Fig. 3). This step is critical in ensuring that the behavior of antenna and radio systems do not interact and create interference. Shawn Carpenter, director of sales and marketing for Delcross Technologies, states,  “Co-site analysis is important anywhere you have collocated RF systems that have the potential to talk to one another in a destructive way. There are several things you have to worry about when you are trying to determine how multiple RF systems work and play together.”

Software offerings like Delcross’s EMIT use asymptotic electromagnetic (EM) analysis to acquire a superposition of currents stimulated across a multi-radio platform. This analysis involves the combining of physical-optics and EM-analysis techniques. First, rays are shot at the geometries of the platform. The circulation currents that were created are analyzed. An observer is then created spatially. It integrates the generated currents, which are transformed into an approximation of far-field contributions at some combination of angles.

Next, the software integrates the antenna, radio, cable, and filter models to define the interaction of these different radios. This can be done channel by channel, component by component, or in complete simulation mode, which Carpenter refers to as a “shooting match.” The goal of the software is to follow the design of a radio system that is intended to operate in a multi-radio platform—from early conception to final design. Such a process could indicate whether certain design decisions will produce interference and compromise the functionality of the various radio systems.

Related Articles
Millimeter-Wave Technology Prepares For A Wealth Of Applications
Satellites Prove Key To Search
Multifunction Test Sets Target Wireless Devices

From antenna interference to chip-level component analysis, advanced system-level-modeling and analysis tools can provide valuable insight throughout the design process. If a system model is well defined and iteratively improved throughout the cycle, costly redesigns can be avoided. The test/verification process can be minimized as well. Thanks to the development of multi-domain tools and the improvements in those tools’ computational efficiency, more refined simulations of complex systems are now possible.

Of course, cost and return-on-investment (ROI) always must be considered when evaluating these often-high-priced tools. In addition, some designs would benefit from having access to multiple modeling tools so that designers could compare and contrast performance. So far, there are no complete start-to-finish tools that account for every aspect of a design. As a result, much weight is still placed on the experience and diligent planning of system architects.

Download this article in .PDF format
This file type includes high resolution graphics and schematics when applicable.

Sponsored Recommendations

In-Circuit Antenna Verification

April 19, 2024
In this video, Brian Walker, Senior RF Design Engineer at Copper Mountain Technologies, shows how there can be significant variation of the performance of a PCB-mounted antenna...

UHF to mmWave Cavity Filter Solutions

April 12, 2024
Cavity filters achieve much higher Q, steeper rejection skirts, and higher power handling than other filter technologies, such as ceramic resonator filters, and are utilized where...

Wideband MMIC Variable Gain Amplifier

April 12, 2024
The PVGA-273+ low noise, variable gain MMIC amplifier features an NF of 2.6 dB, 13.9 dB gain, +15 dBm P1dB, and +29 dBm OIP3. This VGA affords a gain control range of 30 dB with...

Fast-Switching GaAs Switches Are a High-Performance, Low-Cost Alternative to SOI

April 12, 2024
While many MMIC switch designs have gravitated toward Silicon-on-Insulator (SOI) technology due to its ability to achieve fast switching, high power handling and wide bandwidths...