Main Support:       Knowledge Center
Documentation:   IC-CAP English Doc   >  Previous Supported Releases   >  IC-CAP 2014.04   >  IC-CAP 201404 Quick Install and License Setup   >  IC-CAP 201404 Quick Install-Windows

This document contains references to Agilent Technologies. Agilent's former Test and Measurement business has become Keysight Technologies. For more information, go to www.keysight.com.


 

Quick Install - Windows

IC-CAP can be installed on a computer running Windows by downloading the IC-CAP install file from Keysight EEsof EDA website.

Obtain IC-CAP License File

IC-CAP requires a license to run. You can either apply for an Evaluation or a Purchased license. Once the license request is approved, a license file (with .lic extension) is sent as an email attachment. Save this file on your computer at C:\Program Files\Agilent\EEsof_License_Tools\bin\licenses.

Supported Platforms

For details on Supported Platforms, refer to the Supported Platforms section.

System Requirements

The following are Keysight recommended configurations:

CPU

Intel Pentium © 4 or higher, AMD XP 3000 or higher.

Display

High-resolution color only (Super VGA, 1024x768, 15-inch monitor minimum and at least 1280x1024 is required for Extraction packages).

RAM

Minimum is 2 GB RAM, recommended is 3 GB RAM. Minimum 3 GB RAM is required for Windows 7.

Acrobat Reader

Acrobat Reader 5.0 or higher to view the PDF files.

Hard Disk

1.5 GB for complete installation.

Compiler

(Only for user-compiled code interface or open measurement interface). C++ and C: Microsoft Visual Studio .NET 2008 with SP1/Hotfix.

Supported Instrument Interfaces

If you are using IC-CAP with an NI or Keysight GPIB interface, install the interface and its driver according to the instructions provided with the interface.

Description

Part Number

TAMS L488 GPIB/LAN Interface and Keysight IO Libraries version 14.2

L488
L488-POE1

Keysight GPIB PCI card and Keysight IO Libraries

82350A1/B

Keysight LAN/GPIB Gateway Interface and Keysight IO Libraries

E5810A2

Keysight USB/GPIB converter and Keysight IO Libraries

82357A1/B

National Instruments PCMCIA-GPIB card and NI-488.2M drivers

778034

National Instruments PCI-GPIB card and NI-488.2M drivers 3

778032

  1. This is a discontinued product.
  2. Typically, LAN has some impact on speed; therefore, it could be slower than a card.
  3. Keysight IO Libraries can substitute for the NI-488.2M drivers.

    Note

    For the latest information, refer to this manual on our website at: http://www.keysight.com/find/eesof-docs.

For information on how to configure driver for GPIB interface, refer to the Configuring the Driver for the GPIB Interface section.

Download IC-CAP Installer

Click http://www.keysight.com/find/eesof-iccap-latest-downloads to download the installer.

Install IC-CAP

To install IC-CAP, you must have system administrator privileges. Run the downloaded installer and follow the guided tour to complete the installation.

IC-CAP License Setup

At the end of installation, the License Setup Wizard starts automatically after detecting that you do not have a valid license to start IC-CAP. If you choose to skip the license setup, you can complete the process later by clicking Start > Programs > IC-CAP <release_number> > IC-CAP Tools > IC-CAP <release_number> License Manager.

The License Manager has been introduced in the product releases starting October 2012. It is one-stop shop for all licensing tools.

Node-locked License

To setup a counted license, select the Add or replace a license file option and follow the guided tour to complete the license setup process. In case of a USB dongle, attach the dongle to the USB port and invoke the License Manager to complete the setup process.

You must have system administrator privileges to setup node-locked licenses (Only) on Windows Vista and Windows 7 machines.

Floating License

To setup a floating license, select the Add or replace a network license server option and follow the guided tour to complete the license setup process. Consult your license administrator for the network path of the license server.

Launch IC-CAP

To run IC-CAP, go to the Start menu and choose Programs > IC-CAP <release_number> > IC-CAP <release_number> .

 

See Also

 

 

Please help us improve
Please help us improve
Was this topic helpful?