Starting Download..
save Save

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?

This behavior is observed because a PC is needed initially to load the necessary driver into the USB modular instrument or USB DAQ module so it will be recognized as a USB-TMC-488.2 class device. An interim solution for this issue is to establish the connection between the USB modular instrument or USB DAQ module and the PC directly so the driver is loaded properly. Next, disconnect the USB modular instrument or USB DAQ module from the PC (while it’s still powered-on), and subsequently connect it to the E5810B. Now, the USB modular instrument or USB DAQ module will be recognized as a USB-TMC-488.2 class device by the E5810B and the remote USB client on the PC connected to the E5810B.

Learn more about Keysight Data Acquisition (DAQ).

Was this helpful?


Didn't find what you're looking for?