Technical Overviews
Keysight Technologies
Enhanced Display Package Option
EDP X-Series Signal Analyzers and EMI Receiver
Enhanced Display Package
Offering deeper insight to measurement results
The Keysight Technologies, Inc. X-Series signal analyzers provide optimized RF performance including dynamic range, accuracy, and measurement speed at a variety of price points to best suit your measurement needs. In addition, the enhanced display package (Option EDP) available for X-Series signal analyzers is a valuable tool to help you visualize, analyze, and interpret results for effective troubleshooting.
Option EDP is available for all the X-Series signal analyzers including the PXA, MXA, EXA, and CXA and comes standard in the MXE EMI receiver. It is activated by a license-key without requiring any additional hardware. Option EDP adds three display views to the analyzer: spectrogram, trace zoom, and zone span. The additional display views can be found in the graphic user interface as additional soft-keys under the “View/Display” menu (Figure 1).
Spectrogram
The spectrogram view is a visual representation of the spectrum trace of an RF signal as it varies with time. Under the spectrogram view, the display splits into two windows—the standard spectrum trace is at top and the spectrogram window at bottom. In the spectrogram window, spectrum trace history is displayed. Each horizontal line in the spectrogram display represents one historical trace. The data streams upwards from newest to oldest; the latest trace displays on the bottom and the oldest trace on the top (Figure 2).
The spectrogram view provides a quick look at a history of 300 traces. Since this is swept spectrum analysis, each horizontal line in the spectrogram represents a single trace, and the vertical axis represents time. The colors in the spectrogram represent signal amplitude. The key to these colors is displayed next to the Y-Axis in the upper window. A user can define the color scale (hue) to obtain the optimized color contrast.
Under spectrogram view, most functions and settings work the same as the standard display view, including the marker functions which enable quantitative analysis for the events. The spectrogram is particularly useful in visualizing signals such as low-rate FM and in quantifying the time sequence of frequency hopping signals.
Trace zoom
In the trace zoom view, the screen is split into two windows. The top window is a standard spectrum analyzer window, and the bottom window, or zoom window, shows a close-up representation of the traces in the top window (Figure 3). The data in both windows is identical, but the bottom window typically shows fewer data points, spread across the whole display, which allows users to see the data in those points more clearly, particularly when the trace data in the top window is very dense.
The zoom region is indicated by blue shading over that region. The top window indicates which subset of the data is being magnified in the bottom window. The entire zoom window is shaded, to identify that it represents the close-up view of the shaded region in the top window.
It is important to understand that the data and state in the two windows are identical. The zoom window is simply a close-up view of a segment of the traces in the top window. Therefore all traces and markers are the same in both windows; and any state changes you make will affect them both.
The trace zoom display mimics the zoom functions of a camera—it stretches out a region with crowded signals to help you better visualize signals of interest. Customers working on electromagnetic interference (EMI) testing find this feature most helpful when analyzing the interference signals that are close to each other in frequency domain.
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.