Column Control DTX

Generate Looped Test Patterns or PRBS Signals with a Preamble

Application Notes

Problem statement

Some digital integrated circuits (IC) use special modes to test all the internal states of operation. To get into such a mode the IC requires a defined command be sent to the device under test (DUT). As shown in Figure 1, in some instances a portion of the test pattern is used once to advance the special IC mode to an area of operation that requires repetitive use of a test pattern in order to thoroughly test the device.

 

It is very important that the test pattern and the preamble are correctly timed and generating such a sequence may not be a trivial task. If the test pattern is not received at the necessary time, the device can time out and return into a pre-defined state, delaying testing, because the preamble must be rerun to bring the DUT back into the desired test mode.

×

Please have a salesperson contact me.

*Indicates required field

Preferred method of communication? *Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX