Starting Download..
save Save

Can the B2900A Series of SMU sweep voltage source by the know on the front panel?

In the default setting, the source value becomes effective on the B2901/02/11/12A after setting the value and fixing it by the operation such as pressing the rotary knob, the assist keys, etc. At that moment, the status changes to MOVE (blue).
However, once Immediate V/I Update function is enabled, the output will be stepped whenever you change the source value by rotary knob even in the EDIT (green) status.

Please refer to the link below in detail.
How to enable Immediate V/I Update Function

Was this helpful?


Didn't find what you're looking for?