Starting Download..
save Save

How can I find the power-on state setting of the B2961A/B2962A?

The power-on state can be selected from the factory default reset condition (RST) and user conditions (RCL0, RCL1, RCL2, RCL3, and RCL4) which can be defined by using the “*SAV” command.

You can find the power-on state setting on the System Start-up dialog box.
The dialog box is opened by pressing the System>Start-up functuion keys.

Please see the following material for the details.
How to find Power-on State Setting on B2961A/B2962A

Was this helpful?


Didn't find what you're looking for?