How much programming compatibility does exist between 81101A, 81104A, 81110A and 81150A, 81160A?
The implemented 81150A, 81160A SCPI command set is based on Keysight's 81101A, 81104A, 81110A Pulse Pattern Generator product family. Therefore, most of the commands available for that instrument family are also available in the 81150A, 81160A models. The table starting on page 665 in the 81150A and 81160A User's Guide lists the SCPI commands which are not available in 81150A, 81160A as compared to the above-mentioned instruments.