Is there a way to transfer sets of waveforms to each signal generator without having to connect the N7609B software to each instrument?
Yes. All of the waveform files are available on your PC when you install the N7609B application; they are in the application SW folder (default location is C:\Program Files (x86)\Keysight\Signal Studio\Real-time Global Navigation Satellite System\Application\Gnss\Waveform). You can use the Web interface to FTP the required waveform files into the SECUREWAVE directory of each signal generator.