Column Control DTX

Addressing the Challenges of Deploying Single Frequency Networks DVB-T & DVB-T2

Application Notes

Single Frequency Network (SFN) television broadcasting systems have been widely deployed, especially for OFDM based systems like DVB-T and DVB-T2 [1][2], DTMB, and ISDB-T, due to their high frequency efficiency and simple frequency planning. However, building a successful SFN system is challenging because it requires precise transmitter deployment in order to ensure good coverage.

In an SFN, two or more transmitters radiate the same signal on the same frequency simultaneously and repeaters are used to ensure good signal coverage. The receiver is thus likely to receive multiple echoes from many of these transmitters. Echo scenarios in SFN systems in the real world can generally be categorized as one of the following: post-echoes, pre-echoes, pre-echoes and post-echoes.

For an OFDM system, a guard interval (GI) is inserted between symbols to prevent inter-symbol-interference (ISI). As long as the maximum delay of the echoes is within the GI, there should theoretically be no ISI. The principle behind SFN deployment is that the echoes from different transmitters must lie within the GI and echoes outside the GI must be low enough to avoid detection so that no interference is received. 

×

Please have a salesperson contact me.

*Indicates required field

Preferred method of communication? *Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX