Choose a country or area to see content specific to your location
Application Notes
From R&D and manufacturing, to maintenance and repair services, power measurements are ubiquitous in the RF and microwave world. Along with their growing presence, the need to perform peak power measurements is increasing, especially in military and communication applications. These measurements are necessary to test the pulsed transmissions of radar, GSM and WiMAX™ communication devices, and TD-LTE base stations.
While traditional transmission testing in the field has typically relied on the use of a laptop PC, Keysight Technologies’ N934XC handheld spectrum analyzer (HSA) and U2020 X-Series peak power sensors offers an alternative solution which makes testing transmissions easier. For example, when you’re working in field, the long boot-up time for a laptop PC can be an inconvenience. Additionally, laptop PC software typically includes capabilities, such as multiple channels, feeds, and traces mathematics—functionality that is mainly desired by labs and production lines instead of field applications. The N934xC HSA-based solution provides streamlined functions to address the specific needs of the field engineer. That purpose-driven focus is another reason the N934xC/U2020 X-series solution makes peak power measurement setup in the field simpler.
Unlock Content
Sign up for free
*Indicates required field
Thank you.
Your form has been successfully submitted.
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.