Flyers
Keysight Technologies Oscilloscopes in R&D
Stimulus-Response Testing Using an Oscilloscope with Built-in AWG
The Keysight Technologies, Inc. InfiniiVision 3000T, 4000, and 6000 X-Series oscilloscopes can be optionally configured with a built-in function generator with arbitrary waveform generation capability to help you more efficiently test your prototype designs under worst-case input conditions.
R&D hardware designers use a broad range of test and measurement equipment to test their prototype designs. The core instrument used to test the dynamic behavior of both transmitted and received signals is usually an oscilloscope. But to test designs under varied input signals conditions typically requires a signal source as well.
Nearly all electronic designs can be simplified down into transmitter circuits and receiver circuits. Although the receiver half of your design may respond correctly when stimulated by the existing transmitter half of your design, what if the signals generated by the transmitter circuitry exhibited characteristics that barely meet minimum output drive requirements? It’s not a trivial task to “dumb down” your transmitter circuitry in order to generate output signals with worst-case characteristics so that you can test your receiver circuitry under marginal input conditions. A more efficient testing method is to temporarily replace the transmitter half of your design with an arbitrary waveform generator (AWG) that is able to produce signals that closely emulate the complex characteristic of your output signals.
There are various ways to create complex waveforms to download into an AWG, including building a waveform from scratch using an off-line AWG waveform editor on your PC. But perhaps the fastest and easiest method is to simply capture a known good waveform on an oscilloscope, and then transfer the waveform into the AWG for regeneration and modification.
With Keysight’s 3000T, 4000 and 6000 X-Series oscilloscopes, the process of transferring a captured scope waveform into AWG memory is practically automatic since this scope comes with an optional built-in AWG (dual AWG in the 4000 and 6000 X-Series). A PC is not required. Storing the scope waveform in a .CSV format and then importing the file into the AWG is not required. Simply capture the reference waveform on one of scope’s input channels, and then press the Store Source to Arb softkey. Let’s now walk through a stimulus-response measurement example. Figure 1 shows an example of the InfiniiVision X-Series scope capturing three serial packets on its channel-1 input. This complex signal represents a known good output signal from the transmitter part of a design.
Figure 2 shows the AWG editor screen after the waveform has been transferred from internal scope memory into AWG memory. Remember, transferring the waveform from scope memory into AWG memory only requires that you press the Store Source to Arb softkey shown in the lower right-hand corner of this screen image. However, the waveform was originally scaled, captured, and displayed on the scope’s screen (refer to Figure 1) is exactly what is transferred into the AWG’s waveform memory.
The upper blue trace represents the entire waveform memory of the AWG. The lower blue trace shows a zoomed-in portion of the stored waveform. This makes it easy to edit specific points (add points, delete points, modify voltage levels of specific points) using the scope’s built-in AWG waveform editor. But for this particular stimulus-response measurement example, we don’t need to edit individual points. To test our receiver for worst-case input signal conditions we need to modify characteristics of the entire waveform. We would like to test our receiver circuitry under reduced amplitude conditions to test the minimum input sensitivity and add noise to the entire waveform to test for worst-case noise immunity of our new design. Note that we can also modify the frequency of the regenerated waveform to also test for baud rate sensitivity.
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.