The channel 2 in the B2902A or B2912A doesn't receive any SCPI commands.
Question:
I believe that the both channels in the B2902A or B2912A support SCPI commands.
However, the channel 2 shows an error and doesn't receive any SCPI commands. Why?
Answer:
The instrument may be configured to use the conventional command set designed for using the existing programs which you created to control existing instruments such as Keithley 2400.
Keithley 2400 doesn't have the channel 2 so that the instrument doesn't support SCPI commands for the channel 2 with this configuration.
Please take the actions described in the material below and configure the instrument to use the default command set which supports all the B2901/02/11/12A functions.