Choose a country or area to see content specific to your location
- Home
- Resources
- Resources
What are you looking for?
Suggested searches
No product matches found - System Exception
Matched content
New Bios 1.20 version to reduce time to load test program across network
Problem Description:
The Hewlett Packard rp5700 PC model may take a longer time to load a test program or startup “Push Button Debug” if the test program resides in the network server. The above symptoms occur on the rp5700 that uses Bios version 1.12.
Solution:
Perform the following steps to improve the loading time:
1. Update the Bios to 1.20 version
2. Re-install Windows Operating System from scratch
Best results may not be achieved if any of the above steps is skipped.
Download the Bios file “SP54250.zip” and perform the update as according to Service Note 3070-88.