Starting Download..
save Save

How do I upgrade my E6607B Wireless Communications Test Set?

Most all of the EXT options that are sold at the time of instrument purchase are also available as an upgrade option. The upgrades in most cases are either Hardware Options or Measurement Applications. The upgrade contents are described in the tables below as Hardware, Software, License Key, or some combination of the three. Hardware retrofit kits will contain the assemblies to be installed as well as the installation instructions. In many cases a license key will be required to activate the hardware option or measurement application. Upgrade options are categorized as:

  • Internal Hardware Upgrades (Ex. Precision Frequency Reference)
  • External Hardware Upgrades (Ex. Rackmount Kits or Hard Transit Case)
  • Complementary Hardware (Ex. Multiport Adapter)
  • Instrument Software (Ex. Instrument Software & Measurement Applications)

Internal Hardware Upgrades:

Before a hardware upgrade is purchased the following steps should be taken:

  1. View the installation instructions by selecting the "Available" links in the tables below for the desired upgrade option.
  2. Determine from the installation instructions the complexity of the installation and whether you will perform the upgrade yourself or have an Keysight Service Center do it for you.

If an upgrade option is going to be installed by an Keysight Service Center, additional labor charges will apply. Your Keysight field engineer can provide an all inclusive quote for this.

All instrument adjustments are automated and require the use of the Keysight Performance Verification & Adjustment Software which is only available at Keysight Service centers or by use of the Voscal service provided by Keysight.

Many hardware upgrades will require the redemption and installation of a license key file to activate the option. Once a redemption certificate is received the license key file can be redeemed at the Keysight Software License Redemption Website

E6607B Internal Hardware Option Upgrades
Option Description Order As eDelivery Installation Note Upgrade Contents Minimum Firmware Adjustments Required1 Additional Requirements Incompatible With Installed By - Installation Time
PFR Precision Frequency Reference E6607BK-PFR Yes Available License Key None Yes None None Service Center - 0.5 Hrs
(0.5 Hrs Verification Time)

External Hardware Upgrades:

E6607B External Hardware Option Upgrades
Option Description Order As eDelivery Installation Note Upgrade Contents Minimum Firmware Adjustments Required1 Additional Requirements Incompatible With Installed By - Installation Time
1CM Rackmount Kit E6607BK-1CM No Available Hardware None None None 1CM, 1CP

Customer - 0.5 Hrs

1CN Front Handle Kit E6607BK-1CN No Available Hardware None None None 1CN, 1CP Customer - 0.5 Hrs
1CP Rackmount unit and handle kit E6607BK-1CP No Available Hardware None None None 1CM, 1CN Customer - 0.5 Hrs
1CR Rack Slide Kit E6607BK-1CR No Available Hardware None None None None Customer - 1.0 Hrs
HTC Hard Transit Case E6607BK-HTC No None Hardware None None None None Customer - 0.5 Hrs
KYB USB Keyboard E6607BK-KYB No None Hardware None None None None Not applicable
MSE USB Mouse E6607BK-MSE No None Hardware None None None None Not applicable

 Complementary Hardware:

E6607B Complementary Hardware
Option Description Order As eDelivery Installation
    Note
 Upgrade
Contents
Minimum
Firmware
Adjustments
  Required
  Additional
Requirements
Incompatible
     With
Installed By -
Installation Time
E6617A

Multiport Adaptor for        
EXT                           

E6617A            No Available             Hardware           A.09.47             None                              None                                   None                 Customer - 0.5 Hrs         

Instrument Software

Instrument Software Update:

The software update package for the EXT Wireless Communications Test Set contains the X-series analyzer measurement application, all the advanced measurement application software, and all other updates required by the individual measurement assemblies inside the instrument.

Keysight recommends updating the instrument software version whenever an internal hardware upgrade or measurement application is installed into the EXT.

The latest revision of the instrument software installer can be found at:

Measurement Applications:

To see the complete list of software measurement applications available for the EXT Wireless Communications Test Set see:

Measurement Applications require the redemption and installation of a license key file (.lic). Measurement application upgrades are meant to be performed by the customer, and no adjustments or performance verification tests are required.

In order to redeem a license key, the end user must have a valid redemption certificate and then go to the Keysight Software License Redemption Website

Was this helpful?


Didn't find what you're looking for?