How do a take a sweep with both the Quasi-Peak and EMI Average detector at the same time with an MXE EMI Receiver?
While in the Spectrum Analyzer mode there is a restriction of using only one of the EMI detectors (Quasi-peak, EMI Average, CISPR RMS) at a time. However, in the EMI Receiver mode this restriction does not apply. You can use two different EMI detectors, along with either the Peak or Negative Peak detector, for a total of three different detectors at once.