Starting Download..
save Save

Why do I continue to get the "Align 20 Hz to 3.6 GHz Required" message even though I ran the Align Now, All routine on my MXE?

With instrument software versions prior to A.13.25, although the alignment that you ran is called "All" it still does not run all of the instrument alignments in the MXE. There are also RF Preselector alignments that need to be run on a periodic basis. These can be found under the System, Alignments, More, RF Preselector, Align Now menu.

With instrument software version A.13.25 and newer the RF Preselector alignments are included with the Align Now, All routine.

Was this helpful?


Didn't find what you're looking for?