How can I find the remote control command setting of the B2901/02/11/12A?
The Keysight B2901/02/11/12A supports two remote control command sets. One is the default command set which supports all B2901/02/11/12A. The other is the conventional command set designed for using the existing programs which you created to control existing instruments such as Keithley 2400.
You can find the remote control command setting by pressing the System>SCPI functuion keys.
Please see the following material for the details.